2024-05-14 07:32 AM
Dear engineers,
I hope this message finds you well. I am currently encountering an issue with the internal connection feature from DAC to ADC in CubeMX. Specifically, I cannot locate the ADC2 IN16 in the interface, and upon setting up the IN17: VDAC1_OUT2 Channel, CubeMX continuously loads without completing the process.
I have attempted to resolve this issue by using different versions of CubeMX, starting a new project, and even testing it on various computers, yet the problem persists. Could this be a bug in the software, or might I be missing a step in the setup process?
Thank you for looking into this matter and for your ongoing support.
Solved! Go to Solution.
2024-07-05 06:50 AM
Hello @RadekS
This issue is solved on the new release of the STM32CubeMX (V6.12.0).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-14 07:52 AM
Hello,
Could you please indicate which STM32H7 exact part number are you using?
2024-05-14 07:54 AM
Hello @RadekS and welcome to the ST Community 😊.
Could you please add more details on your description (What MCU are you using? Can you add more details? Can you add a .ioc file that reproduce the issue elaborated using the Last CubeMX version (V6.11.1).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-14 08:31 AM
Thank you very much for your response.
The version of the IDE: STMicroelectronics STM32CubeIDE 1.15.1
The version of the CubeMX: 6.11.1-RC2
The chip I working on is: STM32H723ZG
FW HW: STM32Cube FW_H7 V1.11.2
You can (hopefully) reproduce the issue by:
1) File -> New -> STM32 Project
2) Choose the MCU: STM32H723ZGT6
3) Finish the configuration of the project. Accept the default configuration.
Now we can see that ADC2 IN16 is missing.
4) Set up the DAC1_OUT2 to peripherals:
5) Setting the ADC2 IN17 leading to infinite loading:
Saving the ioc file now break the application as you cannot do anything anymore.
I attach the .ioc file of this new project before changing the IN17.
Thank you very much for cooperation.
2024-05-14 08:55 AM - edited 2024-05-14 11:03 AM
Hello @RadekS
I've been able to reproduce this issue and I've report it to the concerned team for correction (under internal ticket number 181386).
Thanks again for reporting.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-14 11:40 AM
Thank you for promptly addressing the issue I reported. I appreciate your efforts in reproducing the problem and escalating it to the concerned team.
While we await a permanent fix, could you please advise if there is a possible workaround or temporary solution that we might employ? Any guidance you can provide would be extremely helpful to maintain our workflow.
Thanks again for your support and cooperation.
2024-05-14 12:20 PM
The workaround until fix is to implement it directly to the code after the generation from CubeMX.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-05 06:50 AM
Hello @RadekS
This issue is solved on the new release of the STM32CubeMX (V6.12.0).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-29 04:16 PM
In CubeMX 6.12.0 for STM32H755BITx, I can not select DAC1_OUT2 to be monitored by ADC IN17. IN17 is not available for section - CubeMX skips from IN16 to IN18.