cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 GPIO Default Behavior

slc2015
Associate II

Hi,

I notice in the STM32H747XIH6 reference manual (RM0399) that 

"During and just after reset, the alternate functions are not active and most of the I/O ports
are configured in analog mode." 

I want to confirm that in "analog mode" the IO is an HZ input without internal pullup or pull-down resistor enabled? Also, can anyone confirm which I/O ports do not assume this behavior on startup (since the RM says most)? 

Thanks!

3 REPLIES 3

The reset value of GPIO registers - see the GPIO chapter in RM - reveals, which pins are not set as default (and also that most pins are in Analog mode with no pullup/pulldown).

JW


@slc2015 wrote:

which I/O ports do not assume this behavior on startup (since the RM says most)? 


Typically, the debug pins are an example.

RomainR.
ST Employee

Hello @slc2015 

I confirm that during and just after  RESET, except for GPIOA and GPIOB, all the others GPIO ports are in an analog mode configuration in GPIOx_MODER with the relevant bits MODERx = 0b11.

When the I/O port is programmed in an analog configuration:
• The output buffer is disabled
• The Schmitt trigger input is deactivated, providing zero consumption for every analog
value of the I/O pin.The output of the Schmitt trigger is forced to a constant value (0).
• The pull-up and pull-down resistors are disabled by hardware and Read access to the input data register gets the value 0

In RM0399 Rev 4, you can refer to section 12.3.13 Analog configuration, especially the Figure 81.

Best regards

Romain,

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.