2022-06-30 8:31 AM
Hi everyone,
I feel like I am running out of options as to why this is occurring as the RM isn't that accurate to setup DMA + PWM using Timers.
The goal is to use TIM15 as a PWM generator running @ 800kHz running until 24 pulses are outputted and then stop until I command it to run again. Within these 24 pulses different duty cycle can occur from 64% for HIGH and 32% for LOW. This TIM15 is using the Repetition Counter register to indicate when 24 pulses as gone by.
What I have working thus far is a nice 24 pulse PWM stream but with only LOW (32%) present even though my buffer that gets transferred to CCR1 contains HIGH values (64%)
The configuration for the TIM15 are as fellow:
LL_DMA_InitTypeDef WS2812B_Config_DMA;
LL_GPIO_InitTypeDef WS2812B_Config_GPIO;
LL_TIM_InitTypeDef WS2812B_Config_TIM15;
LL_TIM_OC_InitTypeDef WS2812B_Config_OC;
LL_TIM_BDTR_InitTypeDef WS2812B_Config_BDTR;
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_TIM15);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
LL_TIM_StructInit(&WS2812B_Config_TIM15);
LL_TIM_OC_StructInit(&WS2812B_Config_OC);
LL_TIM_BDTR_StructInit(&WS2812B_Config_BDTR);
LL_GPIO_StructInit(&WS2812B_Config_GPIO);
LL_DMA_StructInit(&WS2812B_Config_DMA);
//Configure GPIO
WS2812B_Config_GPIO.Alternate = LL_GPIO_AF_4;
WS2812B_Config_GPIO.Mode = LL_GPIO_MODE_ALTERNATE;
WS2812B_Config_GPIO.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
WS2812B_Config_GPIO.Pin = LL_GPIO_PIN_2;
WS2812B_Config_GPIO.Pull = LL_GPIO_PULL_DOWN;
WS2812B_Config_GPIO.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
LL_GPIO_Init(GPIOA, &WS2812B_Config_GPIO);
//Configure DMA
WS2812B_Config_DMA.Direction = LL_DMA_DIRECTION_MEMORY_TO_PERIPH;
WS2812B_Config_DMA.FIFOMode = LL_DMA_FIFOMODE_DISABLE;
WS2812B_Config_DMA.MemBurst = LL_DMA_MBURST_SINGLE;
WS2812B_Config_DMA.MemoryOrM2MDstAddress = (uint32_t)WS28128B_BUFF;
WS2812B_Config_DMA.MemoryOrM2MDstDataSize = LL_DMA_MDATAALIGN_HALFWORD;
WS2812B_Config_DMA.MemoryOrM2MDstIncMode = LL_DMA_MEMORY_INCREMENT;
WS2812B_Config_DMA.Mode = LL_DMA_MODE_NORMAL;
WS2812B_Config_DMA.NbData = MAX_BUFF;
WS2812B_Config_DMA.PeriphBurst = LL_DMA_PBURST_SINGLE;
WS2812B_Config_DMA.PeriphOrM2MSrcAddress = (uint32_t)&TIM15->CCR1;
WS2812B_Config_DMA.PeriphOrM2MSrcDataSize = LL_DMA_PDATAALIGN_HALFWORD;
WS2812B_Config_DMA.PeriphOrM2MSrcIncMode = LL_DMA_PERIPH_NOINCREMENT;
WS2812B_Config_DMA.PeriphRequest = LL_DMAMUX1_REQ_TIM15_UP;
WS2812B_Config_DMA.Priority = LL_DMA_PRIORITY_LOW;
//Interrupt: DMA
LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_4);
NVIC_EnableIRQ(DMA1_Stream4_IRQn);
NVIC_SetPriority(DMA1_Stream4_IRQn, 0);
NVIC_EnableIRQ(TIM15_IRQn);
NVIC_SetPriority(TIM15_IRQn, 0);
LL_DMA_Init(DMA1, LL_DMA_STREAM_4, &WS2812B_Config_DMA);
WS2812B_Config_TIM15.Autoreload = (240e6/WS2812B_FREQ) - 1;
WS2812B_Config_TIM15.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;
WS2812B_Config_TIM15.CounterMode = LL_TIM_COUNTERMODE_UP;
WS2812B_Config_TIM15.Prescaler = 0;
WS2812B_Config_TIM15.RepetitionCounter = MAX_BUFF - 1;
LL_TIM_Init(TIM15, &WS2812B_Config_TIM15);
WS2812B_Config_OC.CompareValue = 0;
WS2812B_Config_OC.OCIdleState = LL_TIM_OCIDLESTATE_LOW;
WS2812B_Config_OC.OCMode = LL_TIM_OCMODE_PWM1;
WS2812B_Config_OC.OCNIdleState = LL_TIM_OCIDLESTATE_LOW;
WS2812B_Config_OC.OCNPolarity = LL_TIM_OCPOLARITY_HIGH;
WS2812B_Config_OC.OCNState = LL_TIM_OCSTATE_DISABLE;
WS2812B_Config_OC.OCPolarity = LL_TIM_OCPOLARITY_HIGH;
WS2812B_Config_OC.OCState = LL_TIM_OCSTATE_ENABLE;
LL_TIM_OC_Init(TIM15, LL_TIM_CHANNEL_CH1, &WS2812B_Config_OC);
WS2812B_Config_BDTR.AutomaticOutput = LL_TIM_AUTOMATICOUTPUT_DISABLE;
WS2812B_Config_BDTR.Break2Filter = LL_TIM_BREAK2_FILTER_FDIV1;
WS2812B_Config_BDTR.Break2Polarity = LL_TIM_BREAK2_POLARITY_LOW;
WS2812B_Config_BDTR.Break2State = LL_TIM_BREAK2_DISABLE;
WS2812B_Config_BDTR.BreakFilter = LL_TIM_BREAK_FILTER_FDIV1;
WS2812B_Config_BDTR.BreakPolarity = LL_TIM_BREAK_POLARITY_LOW;
WS2812B_Config_BDTR.BreakState = LL_TIM_BREAK_DISABLE;
WS2812B_Config_BDTR.DeadTime = 0;
WS2812B_Config_BDTR.LockLevel = LL_TIM_LOCKLEVEL_OFF;
WS2812B_Config_BDTR.OSSIState = LL_TIM_OSSI_DISABLE;
WS2812B_Config_BDTR.OSSRState = LL_TIM_OSSR_DISABLE;
LL_TIM_BDTR_Init(TIM15, &WS2812B_Config_BDTR);
LL_TIM_OC_EnablePreload(TIM15, LL_TIM_CHANNEL_CH1);
LL_TIM_EnableARRPreload(TIM15);
LL_TIM_EnableDMAReq_UPDATE(TIM15);
LL_TIM_EnableIT_UPDATE(TIM15);
LL_TIM_GenerateEvent_UPDATE(TIM15);
LL_TIM_ClearFlag_UPDATE(TIM15);
LL_TIM_EnableAllOutputs(TIM15);
The interrupts that are currently active are DMA1_Stream 4 Transfer Complete & TIM15_Update. For the DMA, I just clear the TC4 interrupt to indicated that everything from the buffer has been transferred over to CCR1 and clear it.
The TIM15_Update interrupt indicates that 24 pulses has gone and I handle it accordingly
The interrupts in how they are setup are as fellow:
extern "C" void DMA1_Stream4_IRQHandler() {
if (LL_DMA_IsActiveFlag_TC4(DMA1)) {
LL_DMA_ClearFlag_TC4(DMA1);
}
}
extern "C" void TIM15_IRQHandler() {
if (LL_TIM_IsActiveFlag_UPDATE(TIM15)) {
LL_TIM_ClearFlag_UPDATE(TIM15);
LL_TIM_DisableCounter(TIM15);
LL_DMA_DisableStream(DMA1, LL_DMA_STREAM_4);
WS2812B::block = false;
}
}
The buffer contents that I've been using:
LOW = 0x5F = 32% duty cycle
HIGH = 0xBF = 64% duty cycle
WS28128B_BUFF[0] uint32_t 0x5f (Hex)
WS28128B_BUFF[1] uint32_t 0x5f (Hex)
WS28128B_BUFF[2] uint32_t 0x5f (Hex)
WS28128B_BUFF[3] uint32_t 0x5f (Hex)
WS28128B_BUFF[4] uint32_t 0xbf (Hex)
WS28128B_BUFF[5] uint32_t 0xbf (Hex)
WS28128B_BUFF[6] uint32_t 0x5f (Hex)
WS28128B_BUFF[7] uint32_t 0x5f (Hex)
WS28128B_BUFF[8] uint32_t 0x5f (Hex)
WS28128B_BUFF[9] uint32_t 0x5f (Hex)
WS28128B_BUFF[10] uint32_t 0x5f (Hex)
WS28128B_BUFF[11] uint32_t 0x5f (Hex)
WS28128B_BUFF[12] uint32_t 0x5f (Hex)
WS28128B_BUFF[13] uint32_t 0x5f (Hex)
WS28128B_BUFF[14] uint32_t 0x5f (Hex)
WS28128B_BUFF[15] uint32_t 0x5f (Hex)
WS28128B_BUFF[16] uint32_t 0x5f (Hex)
WS28128B_BUFF[17] uint32_t 0x5f (Hex)
WS28128B_BUFF[18] uint32_t 0x5f (Hex)
WS28128B_BUFF[19] uint32_t 0x5f (Hex)
WS28128B_BUFF[20] uint32_t 0x5f (Hex)
WS28128B_BUFF[21] uint32_t 0x5f (Hex)
WS28128B_BUFF[22] uint32_t 0x5f (Hex)
WS28128B_BUFF[23] uint32_t 0x5f (Hex)
Picture of logic analyzer
Why arent I seeing my HIGHs ?
Solved! Go to Solution.
2022-06-30 2:04 PM
My guess: because the DMA is triggered after 24 pulses, not on every pulse, as a result of using repetition counter. Also, make sure that CCR1 is buffered.
Another problem: the buffer contains 32-bit data, but DMA is programmed for 16-bit words.
Honestly, there are at least two more efficient ways to output WS2812 data - using UART or SPI.
2022-06-30 2:04 PM
My guess: because the DMA is triggered after 24 pulses, not on every pulse, as a result of using repetition counter. Also, make sure that CCR1 is buffered.
Another problem: the buffer contains 32-bit data, but DMA is programmed for 16-bit words.
Honestly, there are at least two more efficient ways to output WS2812 data - using UART or SPI.
2022-07-01 1:25 AM
Hi! You were completely right as I misunderstood what repetition meant, quickly corrected that by returning that register to 0x00.
Corrected for the DMA already, good eye.
Sure, but i mean its easier to implement