2024-07-16 10:37 PM - edited 2024-07-16 10:49 PM
Hi Experts,
Is it possible to use STM32H5 OctoSPI interface (configured as Dual-Single-SPI) as two individual transmit-only SPI masters?
Requirements:
1. Two devices connected to MCU are identical but receive different data
2. Devices are not a memory
3. No data needs to be received by MCU
4. No simultaneous write is required
If such configuration is possible, how will HAL code look like?
Which of OCTOSPI_IO0, IO1, IO2, IO3 pins are can be configured as 'MOSI'?
Edit: I realized 'Dual SPI' and 'Dual-Single SPI' are a different things. Changed post subject to 'Dual-Single SPI'