2024-05-08 10:33 AM
Hello,
does STM32H562 have the system rom bootloader?
I cannot find it AN2606, however its datasheet does mention the system bootloader.
Thank you
Solved! Go to Solution.
2024-09-17 03:16 AM - edited 2024-09-17 03:17 AM
Hello @tommz9
The bootloader of the STM32H562 has been add to the AN2606 on the Revision 63.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-08 10:39 AM
Hi,
reading rm0481 might help :
2024-05-08 11:27 AM
Thanks, yes this is the table I referred to in my original post. However, when I look at AN2606 it does not list STM32H562 as an option. So now I am not sure, is the reference manual wrong? Or AN2606? Or am I reading it wrong?
2024-05-08 11:38 AM - edited 2024-05-09 06:41 AM
Hello @tommz9 and welcome to the ST Community
Thank you for reporting this. It is already reported to the concerned team to update the AN2606 ASAP (under internal ticket number 179001).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-08 12:20 PM - edited 2024-05-08 12:22 PM
STM32H5 series: STM32H503xx, STM32H563xx, STM32H573xx, STM32H523xx, STM32H533xx
I'd wager they share the same die
The H562 lacks Ethernet, well at least that part of the core, and the IP costs associated with it are disabled / deducted.
2024-09-17 03:16 AM - edited 2024-09-17 03:17 AM
Hello @tommz9
The bootloader of the STM32H562 has been add to the AN2606 on the Revision 63.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.