cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H562 bootaloder

tommz9
Associate

Hello,

does STM32H562 have the system rom bootloader?

I cannot find it AN2606, however its datasheet does mention the system bootloader.

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @tommz9 

The bootloader of the STM32H562 has been add to the AN2606 on the Revision 63.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
AScha.3
Super User

Hi,

reading rm0481 might help :

AScha3_0-1715189937422.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Thanks, yes this is the table I referred to in my original post. However, when I look at AN2606 it does not list STM32H562 as an option. So now I am not sure, is the reference manual wrong? Or AN2606? Or am I reading it wrong?

Hello @tommz9 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Thank you for reporting this. It is already reported to the concerned team to update the AN2606 ASAP (under internal ticket number 179001).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdf

STM32H5 series: STM32H503xx, STM32H563xx, STM32H573xx, STM32H523xx, STM32H533xx

I'd wager they share the same die

The H562 lacks Ethernet, well at least that part of the core, and the IP costs associated with it are disabled / deducted.

https://www.st.com/resource/en/reference_manual/rm0481-stm32h52333xx-stm32h56263xx-and-stm32h573xx-armbased-32bit-mcus-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
STTwo-32
ST Employee

Hello @tommz9 

The bootloader of the STM32H562 has been add to the AN2606 on the Revision 63.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.