2024-01-23 06:04 AM - last edited on 2024-01-25 03:49 AM by SofLit
I use STM32H562 and/or STM32H503 (nucleo board). When try in loop only this line:
while (1)
{
GPIOB->ODR ^= GPIO_PIN_6;
}
The frequency on pin is only 12.5 mhz. I use external quartz 8mhz (and 24mhz on nucleo)
I config to 250mhz (with build-in CubeMX ) :
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLL1_SOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 2;
RCC_OscInitStruct.PLL.PLLN = 125;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1_VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1_VCORANGE_WIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
}
Why is output frequency is too low ?. In assembler are no more 5 lines. So must be arround 50mhz.
2024-01-23 06:16 AM
Welcome @Brussl, to the community!
well, a similar issue has already been discussed several times in the community, for example here.
Hope that helps?
Regards
/Peter
2024-01-23 06:41 AM - edited 2024-01-23 06:41 AM
In my speed test on H563 at 250M core , i got
bsrr 4ns , +12ns ( while loop 8+4ns) => 16ns total , so about 62MHz output at a pin, including the while loop.
But only if compiling with optimizer -O2 (or -Ofast) , these cpus are made to be fast only in cooperation with the optimized code. So set the optimizer...
2024-01-23 08:24 AM
Tnx a lot for fast answers. I see and other strange - when i add HAL_Delay(1) in loop the period is not around 2ms but 4ms - 2 time slower !
AScha.3 - Tnx will check it. Can you send me SystemClock_Config(void) function if is different from mine. And what source you have use? And what is VCC - 3.3V?
2024-01-23 08:45 AM - edited 2024-01-23 08:47 AM
To check internal clk, you have a MCO output ! Enable it, select the clock to test and test on mco pin with scope (or counter ) . I did this at first ... never trust anything.
-> testing pll1q (100M) /10 here , 10M coming out.
+ here SystemClock_Config , just as cube puzzeled it together:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS_DIGITAL;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLL1_SOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 250;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 5;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1_VCIRANGE_1;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1_VCORANGE_WIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
cpu at 3v3 , source ...is on NUCLEO-H563ZI board...hse bypass , set :8MHz .
2024-01-23 05:14 PM
The RMW is going to be inherently slow. It's compounded by the speed of the bus.
Do singular writes to BSRR to set a pin high or low.
If you need to toggle a pin use the TIM. Don't saturate the processor and bus.
For driving patterns use DMA from a buffer to the GPIO BSRR register.
2024-01-24 03:43 AM
to AScha.3 : Sorry to say but problem still. Please try with external qaurtz to make 250mhz.
I can't. I use CubeIDE 1.14.1
For example on MB1814 board (STM32H503) with 24mhz quarz:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLL1_SOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 3;
RCC_OscInitStruct.PLL.PLLN = 62;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 50;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1_VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1_VCORANGE_WIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 4096;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_PLL1Q, RCC_MCODIV_1);
}
Max frequency is around 18mhz when use optimization by speed.
Interesting is that on MCO1 pin not signal !!
I try and on other custom board with STM32H562 and result is the same.
This is photos of clock config:
2024-01-25 12:53 AM
Some one to help ? I can't start project 3 days. Just simple 250mhz setup i can't make with extarnal qartz. Where is f..ng problem. I use last lib of stm32H5 1.1.1. My be something in library is not OK!? Why frequency a half of 250 mhz and why on MCO1 pin not signal ? I check frequency of quarts and is 24mhz. So my scope measuring ok.
I see when use HAL_Delay(1) that delay time is not 1 ms but 2ms. SUPER STRANGE !!!
2024-01-25 01:50 AM - edited 2024-01-25 01:55 AM
So first : why on MCO1 pin not signal ? This cannot be...we dont allow!
set mco in Cube (?) ->
then set the mux:
and check : input is the real value on your board ? :
on my H563 nucleo : is 8MHz !
Now check mco1 output ...!
2024-01-25 03:31 AM
I set only in cubeMX. Please measure frequency with HAL_Delay in loop. And if you have output from MCO1 too measure it. I have not output form MCO1. Please check which is your version of HAL. I use last one.1.1