cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G491 datasheet echo!

Andrew Neil
Evangelist III

The sentence "Exposure to maximum rating conditions for extended periods may affect device reliability" is repeated:

AndrewNeil_0-1727438152006.png

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @Andrew Neil 

Thank you so much for reporting this typo. I've report it to the concerned team for correction on the coming releases (under internal ticket number 192316).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Karl Yamashita
Lead III

ST is making sure you didn't miss reading it the first time and it sticks to your memory

KarlYamashita_0-1727454041725.jpeg

 

If smoke escapes your device, put the smoke back in. It'll still work as a conversation piece. If you find my answers useful, click the Accept as Solution button so that way others can see the solution.