2024-08-05 1:03 AM - edited 2024-08-05 1:09 AM
hi,
for our project,we used firmware package was STM32CubeG4 Firmware Package V1.6.0 / 05-June-2024.
IDE: MDK 5.39
MCU: STM32G473MET6 EEPROM: 24LC256
we already check the page write opreation, ensure the boundaries and size of each write (less than or equal to the page size)
we have also tried DMA and IT, but they will affect SYSTICK
this our test code
uint32_t EEPROM_WriteBytes(uint16_t address, uint8_t *pData, uint16_t length)
{
while( (HAL_GetTick() -LastWriteTick) <=6);
LastWriteTick = HAL_GetTick();
if (HAL_I2C_Mem_Write(&hi2c4, _24LCXX_I2C_ADDRESS, address, I2C_MEMADD_SIZE_16BIT,
pData, length, HAL_MAX_DELAY) != HAL_OK)
{
return 0;
}
uint32_t EEPROM_ReadBytes(uint16_t address, uint8_t *pData, uint16_t length)
{
while( (HAL_GetTick() -LastWriteTick) <=6);
if (HAL_I2C_Mem_Read(&hi2c4, _24LCXX_I2C_ADDRESS, address, I2C_MEMADD_SIZE_16BIT,
pData, length, HAL_MAX_DELAY) != 0)
{
return 0;
}
return 1;
}
Solved! Go to Solution.
2024-08-05 9:40 AM
Really shouldn't jump around unless you're trashing the environment.
With Keil make sure you've allocated an adequate STACK (see startup_stm32xyz.s) otherwise in will plough into the HEAP and STATICS/LOCALEs
Watch your local/auto variable allocations and call-depth
2024-08-05 6:22 AM
The systick code is dirt simple. You can inspect it. Unlikely to be bugs there.
Why do you think it's getting changed randomly? What values do you see vs what values do you expect?
2024-08-05 6:59 AM
/**
* @brief This function handles System tick timer.
*/
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
HAL_IncTick();
/* USER CODE BEGIN SysTick_IRQn 1 */
/* USER CODE END SysTick_IRQn 1 */
}
/**
* @brief This function is called to increment a global variable "uwTick"
* used as application time base.
* @note In the default implementation, this variable is incremented each 1ms
* in SysTick ISR.
* @note This function is declared as __weak to be overwritten in case of other
* implementations in user file.
* @retval None
*/
__weak void HAL_IncTick(void)
{
uwTick += uwTickFreq;
}
I know it's easy, that's why I'm confused. The variable 'uwTick' operated by the default code generated by CubeMX mentioned above, when I perform multiple eeprom writes, the value will randomly jump, but after writing, it will count normally.
The "uwTick" variable in the watch window will randomly change, such as suddenly resetting to zero, or suddenly becoming 0x20xxxxxx, or 0x80xxxxxx. However, after the write operation is completed, the variable will count normally based on the changed value
2024-08-05 9:30 AM
Yeah that's a weird one.
If uwTick is getting modified, you can set up a conditional breakpoint and see what instruction is causing the bad behavior. Possibly an out of bounds write.
It could also be an IDE issue, maybe reading from the wrong address. Seems less likely. Consider sending uwTick out via UART or similar to eliminate that possibility.
2024-08-05 9:35 AM
Thank you for providing new troubleshooting directions. If there are any results, I will reply as soon as possible.
2024-08-05 9:40 AM
Really shouldn't jump around unless you're trashing the environment.
With Keil make sure you've allocated an adequate STACK (see startup_stm32xyz.s) otherwise in will plough into the HEAP and STATICS/LOCALEs
Watch your local/auto variable allocations and call-depth
2024-08-05 6:07 PM
Thank you very much. The problem has been solved because the stack is too small
2024-08-05 6:09 PM
Thanks. The problem has been solved