cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4 I/O input high level voltage

JR1
Associate

Dear Sir's,

 

what is the minimum high level threshold voltage

for a non FT_C port? Is it 0.7xVDD or 0.49xVDD+0.26?

2024-03-13_13h09_41.png

 

Regards,

Jochen

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @JR1 and welcome to the community 🙂,

These 2 formulas are correct  VIH = 0.7x VDD is the threshold tested in production and VIH=0.49xVDD+0.3V is the threshold guaranteed by design as mentioned in note 3.

This behavior is mentioned in data sheet figure 25: in blue the threshold level tested in production and in green the threshold level guaranteed by design.

KDJEM1_0-1710332841903.png

May this discussion can help you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Andrew Neil
Evangelist III

What does the note (3) tell you?

AndrewNeil_0-1710332378970.png

 

KDJEM.1
ST Employee

Hello @JR1 and welcome to the community 🙂,

These 2 formulas are correct  VIH = 0.7x VDD is the threshold tested in production and VIH=0.49xVDD+0.3V is the threshold guaranteed by design as mentioned in note 3.

This behavior is mentioned in data sheet figure 25: in blue the threshold level tested in production and in green the threshold level guaranteed by design.

KDJEM1_0-1710332841903.png

May this discussion can help you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.