cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G071 Push Pull PWM and Fault Pin

Karan 123
Senior

Hi,

I​ have control H-bridge with 4 IGBTs . 

PWM Topology : Push Pull Mode

PWM Frequency : 10KHz to 100KHz

Dead Time : 2.5us

Duty Cycle : 0% to 50%

Emergency Stop : 2 Fault Pins for Individual Channels

How to achieve below wave with STM32G071 MCU and STM32CubeMx.

0693W00000WHUFNQA5.pngThe Push-Pull PWM mode alternately outputs the PWM signal on one of two PWM pins

2 REPLIES 2

Search reference manual for "PWM center-aligned mode".

Karan 123
Senior

Hi Michal Dudka (Community Member)

I am gone below Reference manual Page No. 650 and 651 and searched reference manual for

"PWM center-aligned mode".

Where is the detail of Push Pull Mode and Is there any demo code?

STM32G0x1 advanced Arm®-based 32-bit MCUs - Reference manual

0693W00000WHVXwQAP.png0693W00000WHVY6QAP.png 

--

Karan