2024-04-08 09:25 AM - last edited on 2024-04-08 10:06 AM by SofLit
Hello,
According to the datasheet PB7 can be used as ADC_IN11.
Is this an error in datasheet? ADC_IN11 is already used by PB10 and cubeMX doesn't seem to allow me to use PB7 or to remap this pin. How can I use ADC_IN11 on pin PB7 as mentioned in datasheet?
Thanks
Solved! Go to Solution.
2024-04-22 02:52 AM
Hi @AHame,
the DS is unclear as it indicates two possible bondings of the ADC inputs without making the distinction between packages. A decision was made to make the ADC inputs available on smaller packages even if the primary pin dedicated for the function is not available.
So LQFP48 has for example ADC_IN11 bonded to PB10, but as PB10 is not on small packages, the ADC_IN11 is rerouted to PB7 on those. But on LQFP48, ADC_In11 is only on PB10.
I explained the situation to the datasheet responsible and it should be fixed soon.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-22 06:03 AM - edited 2024-04-22 07:16 AM
I read you message again I understand what you mean now. This datasheet is clearly misleading and should indeed be fixed...
2024-04-23 08:53 AM
Internal ticket number 178606 (not accessible by community users).