STM32G031xx: Mistake/Bug in device specific header file???
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 9:54 AM
Hi
so I am trying to get the UART2 on my STM32G031K8Tx up and running. RefManual shows in Chapter 5.4.21 a CCIPR register (Peripherals independent clock configuration register), where bits 2-3 relate to the USART2.
When looking at the device specific header file for the STM32G031xx series, I cannot seem to find the USART2 peripheral clock. In fact, using the LL API from ST, I get a compilation error on the following line:
LL_RCC_SetUSARTClockSource(LL_RCC_USART2_CLKSOURCE_PCLK1);
/******************** Bit definition for RCC_CCIPR register ******************/
#define RCC_CCIPR_USART1SEL_Pos (0U)
#define RCC_CCIPR_USART1SEL_Msk (0x3UL << RCC_CCIPR_USART1SEL_Pos) /*!< 0x00000003 */
#define RCC_CCIPR_USART1SEL RCC_CCIPR_USART1SEL_Msk
#define RCC_CCIPR_USART1SEL_0 (0x1UL << RCC_CCIPR_USART1SEL_Pos) /*!< 0x00000001 */
#define RCC_CCIPR_USART1SEL_1 (0x2UL << RCC_CCIPR_USART1SEL_Pos) /*!< 0x00000002 */
#define RCC_CCIPR_LPUART1SEL_Pos (10U)
#define RCC_CCIPR_LPUART1SEL_Msk (0x3UL << RCC_CCIPR_LPUART1SEL_Pos) /*!< 0x00000C00 */
#define RCC_CCIPR_LPUART1SEL RCC_CCIPR_LPUART1SEL_Msk
#define RCC_CCIPR_LPUART1SEL_0 (0x1UL << RCC_CCIPR_LPUART1SEL_Pos) /*!< 0x00000400 */
#define RCC_CCIPR_LPUART1SEL_1 (0x2UL << RCC_CCIPR_LPUART1SEL_Pos) /*!< 0x00000800 */
#define RCC_CCIPR_I2C1SEL_Pos (12U)
#define RCC_CCIPR_I2C1SEL_Msk (0x3UL << RCC_CCIPR_I2C1SEL_Pos) /*!< 0x00003000 */
#define RCC_CCIPR_I2C1SEL RCC_CCIPR_I2C1SEL_Msk
#define RCC_CCIPR_I2C1SEL_0 (0x1UL << RCC_CCIPR_I2C1SEL_Pos) /*!< 0x00001000 */
#define RCC_CCIPR_I2C1SEL_1 (0x2UL << RCC_CCIPR_I2C1SEL_Pos) /*!< 0x00002000 */
#define RCC_CCIPR_I2S1SEL_Pos (14U)
#define RCC_CCIPR_I2S1SEL_Msk (0x3UL << RCC_CCIPR_I2S1SEL_Pos) /*!< 0x0000C000 */
#define RCC_CCIPR_I2S1SEL RCC_CCIPR_I2S1SEL_Msk
#define RCC_CCIPR_I2S1SEL_0 (0x1UL << RCC_CCIPR_I2S1SEL_Pos) /*!< 0x00004000 */
#define RCC_CCIPR_I2S1SEL_1 (0x2UL << RCC_CCIPR_I2S1SEL_Pos) /*!< 0x00008000 */
#define RCC_CCIPR_LPTIM1SEL_Pos (18U)
#define RCC_CCIPR_LPTIM1SEL_Msk (0x3UL << RCC_CCIPR_LPTIM1SEL_Pos) /*!< 0x000C0000 */
#define RCC_CCIPR_LPTIM1SEL RCC_CCIPR_LPTIM1SEL_Msk
#define RCC_CCIPR_LPTIM1SEL_0 (0x1UL << RCC_CCIPR_LPTIM1SEL_Pos) /*!< 0x00040000 */
#define RCC_CCIPR_LPTIM1SEL_1 (0x2UL << RCC_CCIPR_LPTIM1SEL_Pos) /*!< 0x00080000 */
#define RCC_CCIPR_LPTIM2SEL_Pos (20U)
#define RCC_CCIPR_LPTIM2SEL_Msk (0x3UL << RCC_CCIPR_LPTIM2SEL_Pos) /*!< 0x00300000 */
#define RCC_CCIPR_LPTIM2SEL RCC_CCIPR_LPTIM2SEL_Msk
#define RCC_CCIPR_LPTIM2SEL_0 (0x1UL << RCC_CCIPR_LPTIM2SEL_Pos) /*!< 0x00100000 */
#define RCC_CCIPR_LPTIM2SEL_1 (0x2UL << RCC_CCIPR_LPTIM2SEL_Pos) /*!< 0x00200000 */
#define RCC_CCIPR_TIM1SEL_Pos (22U)
#define RCC_CCIPR_TIM1SEL_Msk (0x1UL << RCC_CCIPR_TIM1SEL_Pos) /*!< 0x00400000 */
#define RCC_CCIPR_TIM1SEL RCC_CCIPR_TIM1SEL_Msk
#define RCC_CCIPR_ADCSEL_Pos (30U)
#define RCC_CCIPR_ADCSEL_Msk (0x3UL << RCC_CCIPR_ADCSEL_Pos) /*!< 0xC0000000 */
#define RCC_CCIPR_ADCSEL RCC_CCIPR_ADCSEL_Msk
#define RCC_CCIPR_ADCSEL_0 (0x1UL << RCC_CCIPR_ADCSEL_Pos) /*!< 0x40000000 */
#define RCC_CCIPR_ADCSEL_1 (0x2UL << RCC_CCIPR_ADCSEL_Pos) /*!< 0x80000000 */
I am not sure, but I suspect that the device specific header file does not match with the reference manual? Or what am I missing here?
Thank you,
- Labels:
-
RCC
-
STM32G0 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 10:46 AM
There is no clock configuration for USART2 on that chip so the USART2SEL field is reserved. There is a note saying it only exists on devices which implement independent clock selection:
And a further note saying STM32G031 is not one of them.
I would argue that the header file is correct not to include that field as it is reserved on that chip and that the real bug here is that CubeMX generates code that tries to access it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 11:54 AM
EDIT:
There was nothing wrong with the code, I measured on the wrong pin by mistake. Sorry
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 3:07 PM
Read out and check/post content of UART and relevant GPIO registers.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 11:45 PM
EDIT:
There was nothing wrong with the code, I measured on the wrong pin by mistake. Sorry