2024-04-19 10:37 AM - last edited on 2024-04-22 03:02 AM by STTwo-32
RM0444 (Rev. 5 Nov 2020 - should be newest):
Chapter 15.8 Oversampler: "N is defined using the OVFS[2:0] bits": this should say "OVSR[2:0]" bits.
Chapter 15.12.3: Register ADC_CR Note for AD_EN: "set ADEN only when all bits of ADC_CR registers are 0" should better say: "set ADEN only when all bits of ADC_CR register except ADVREGEN are 0"
Chapter 15.12.5: Register ADC_CFGR2 A warning hint/Note for OVSR[2:0] would be nice, e. g. : Note: ADC_DR truncates to 16bit (set OVSS to 1-4 shifts for OVSR values 4..7 (32x...256x)).
Solved! Go to Solution.
2024-04-19 11:06 AM - edited 2024-04-22 03:31 AM
Hello @flyer31
Thank you for your contribution. I've escalate this internally for correction for the first proposition and for reviewing by the doc owner for the other two points (under internal ticket number 179616).
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-19 11:06 AM - edited 2024-04-22 03:31 AM
Hello @flyer31
Thank you for your contribution. I've escalate this internally for correction for the first proposition and for reviewing by the doc owner for the other two points (under internal ticket number 179616).
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.