2022-06-29 04:24 AM
Hi,
I'm not able to find any example on STM32CubeIDE about ADC 16-bit oversampling. Could someone from ST provide this for the STM32G0 MCUs?
thanks in advance,
gaston
Solved! Go to Solution.
2022-06-30 03:16 AM
Hi @Gaston ,
If you are using cubemx to configure your project, you can use a generic ADC example for the G0 and then enable oversampling.
Is there a particular aspect that you are looking to clarify?
cheers.
2022-06-30 03:16 AM
Hi @Gaston ,
If you are using cubemx to configure your project, you can use a generic ADC example for the G0 and then enable oversampling.
Is there a particular aspect that you are looking to clarify?
cheers.
2022-06-30 06:19 AM
Thank you for the clarify this.
gaston
2022-07-06 05:26 AM
Hi @Gaston ,
Besides to the proposal from @RetroInTheShade, you can follow this example: https://github.com/STMicroelectronics/STM32CubeG0/tree/master/Projects/NUCLEO-G070RB/Examples_LL/ADC/ADC_Oversampling_Init
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.