STM32F765 ADC reading on channel individual at a time
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-06 12:58 PM
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-06 1:18 PM
It is architected to read multiple channels in a looping fashion into a DMA buffer, with little user interaction and waiting.
You want individual channel sampling, perhaps look at the Injected method.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-06 10:34 PM
Here's my quick (CubeMX and HAL) and not too smart (polling... meh... & CubeMX and HAL :D ) version for F767:
/* Includes ------------------------------------------------------------------*/
#include "adc.h"
ADC_HandleTypeDef hadc1;
float TemperatureMCU = 0.0f;
/* read internal ADC channel */
HAL_StatusTypeDef ADC1_GetAdcVal(uint32_t channel, uint16_t *u16AdcVal)
{
if( ADC1_ChannelSelect(channel) != HAL_OK ) return HAL_ERROR;
if( HAL_ADC_Start(&hadc1) != HAL_OK ) return HAL_ERROR;
if( HAL_ADC_PollForConversion(&hadc1, ADC_TIMEOUT_TEMP_MS) != HAL_OK ) return HAL_ERROR;
*u16AdcVal = (uint16_t)HAL_ADC_GetValue(&hadc1);
if( HAL_ADC_Stop(&hadc1) != HAL_OK ) return HAL_ERROR;
return HAL_OK;
}
/* read internal temperature sensor */
HAL_StatusTypeDef ADC1_GetTempVal(uint16_t *u16TempVal, float *flTempVal)
{
uint32_t u32AdcVal = 0;
float flAdcVal = 0.0f;
if( ADC1_ChannelSelect(ADC_CHANNEL_TEMPSENSOR) != HAL_OK ) return HAL_ERROR;
if( HAL_ADC_Start(&hadc1) != HAL_OK ) return HAL_ERROR;
if( HAL_ADC_PollForConversion(&hadc1, ADC_TIMEOUT_TEMP_MS) != HAL_OK ) return HAL_ERROR;
u32AdcVal = HAL_ADC_GetValue(&hadc1);
*u16TempVal = (uint16_t)u32AdcVal;
if( HAL_ADC_Stop(&hadc1) != HAL_OK ) return HAL_ERROR;
/* calculate temperature, see reference manual */
flAdcVal = (float)u32AdcVal * ADC_VOLT_PER_LSB;
flAdcVal -= (float)ADC_TEMP_SENSE_V25DEG;
flAdcVal /= (float)ADC_TEMP_SENSE_AVG_SLOPE;
flAdcVal += (float)25.0;
*flTempVal = flAdcVal;
return HAL_OK;
}
/* ADC channel select */
HAL_StatusTypeDef ADC1_ChannelSelect(uint32_t Channel)
{
ADC_ChannelConfTypeDef sConfig = { 0 };
sConfig.Channel = Channel;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
uart_printf("Error HAL_ADC_ConfigChannel()\n\r");
return HAL_ERROR;
}
return HAL_OK;
}
/**
* @brief ADC1 Initialization Function
* @param None
* @retval None
*/
void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV8;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
//hadc1.Init.NbrOfDiscConversion = 0;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler_FL(__FILE__, __LINE__);
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_9;
#if(0)
sConfig.Channel = ADC_CHANNEL_3;
sConfig.Channel = ADC_CHANNEL_VREFINT;
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
#endif
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler_FL(__FILE__, __LINE__);
}
}
/**
* @brief ADC MSP Initialization
* This function configures the hardware resources used in this example
* @param hadc: ADC handle pointer
* @retval None
*/
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hadc->Instance == ADC1)
{
/* Peripheral clock enable */
__HAL_RCC_ADC1_CLK_ENABLE();
#if( 0 )
__HAL_RCC_GPIOA_CLK_ENABLE();
/** ADC1 GPIO Configuration
PA3 ------> ADC1_IN3
*/
GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
#endif
__HAL_RCC_GPIOB_CLK_ENABLE();
/** ADC1 GPIO Configuration
PB1 ------> ADC1_IN9
*/
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
}
/**
* @brief ADC MSP De-Initialization
* This function freeze the hardware resources used in this example
* @param hadc: ADC handle pointer
* @retval None
*/
void HAL_ADC_MspDeInit(ADC_HandleTypeDef* hadc)
{
if(hadc->Instance==ADC1)
{
/* Peripheral clock disable */
__HAL_RCC_ADC1_CLK_DISABLE();
/**ADC1 GPIO Configuration
PA0 ------> ADC1_IN0
PA3 ------> ADC1_IN3
*/
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_0|GPIO_PIN_3);
/* ADC1 DMA DeInit */
HAL_DMA_DeInit(hadc->DMA_Handle);
}
}
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-06 10:36 PM
The above code is written in an editor with TAB = 4 spaces, sorry for that ugly piece...