2024-07-17 12:12 AM
Hello,
I have a SPI TX DMA,
and I need to do the following
I guess the last step (6) is not possible ? right ? or is there a way to change the current position
I tried to change it using the __HAL_SET_COUNTER but it is not working
Do I miss something ?
Vincent