cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429IIT6 RTC Abnormal please help me!!

blin.0
Associate II

Hi everyone!! I am from Taiwan

I am currently working on a project that records time using STM32F429IIT6

VBAT is connected to the 3.3V output of the power supply.

PDR_ON is connected to VDD

Power on when VDD is powered off

Time will be initialized

Project output is with STM32CUBE

I really don't know what to do.

please help me

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

What are the symptoms?

What is the initialization code of RTC?

Did you try to look at some of the example projects related to RTC?

JW

blin.0
Associate II

Hi JW

I am trying to print out the value of RTC_BKP_DR0

The value of the first RTC_BKP_DR0 is 0X32F2

Later I changed the value of RTC_BKP_DR0 to 0X1111

Download to the STM32F429IIT6

After NRST is triggered, RTC_BKP_DR0 is still 0X32F2

But after I cut off VDD, I will re-power it. The value of RTC_BKP_DR0 is 0X1111

VBAT has connected to Super capacitor

I don't know if this is normal

RTC_BKP_DR0 should still be 0X32F2, it should not be 0x1111