2024-05-13 06:41 AM - edited 2024-05-13 06:49 AM
Hello together,
even this is freeRTOS related, i hope this is the correct place for my problem.
I have the following Board with an STM32F407VET:
I started from a github repo with a working configuration:
https://github.com/art103/JZ-F407VET6
I removed everything I don't need in my .ioc file, created the code and added the following files to the while()-loop in the main function:
HAL_GPIO_TogglePin(GPIOE, LED1_Pin);
HAL_Delay(500);
HAL_GPIO_TogglePin(GPIOE, LED2_Pin);
HAL_Delay(500);
HAL_GPIO_TogglePin(GPIOE, LED3_Pin);
HAL_Delay(500);
and I can see that the LEDs are changing, so I expect the basic setup is correct.
But as soon as I add freeRTOS to my project, create the code again and add the following code to my only task:
for(;;)
{
osDelay(100);
HAL_GPIO_TogglePin(GPIOE, LED1_Pin);
osDelay(100);
HAL_GPIO_TogglePin(GPIOE, LED2_Pin);
osDelay(100);
HAL_GPIO_TogglePin(GPIOE, LED3_Pin);
osDelay(100);
}
nothing happend, it looks like this Task is never started at all.
I use CMSIS_V2 interface for freeRTOS, changed the USE_NEWLIB_REENTRANT to true and switched under "SYS" the Timebase Source to TIM6.
I use STM32CubeIDE with Version: 1.15.1.
It would be really great if someone could give me a tip as to what I'm doing wrong
2024-05-13 07:30 AM
Hello,
Need to attach your project including the ioc file, so I will try to have a look.
2024-05-13 08:53 AM - edited 2024-05-13 08:54 AM
2024-05-13 09:18 AM - edited 2024-05-13 09:21 AM
Hello,
I've ported your project to STM32F4-Discovery board and I didn't reproduce the issue.
The LEDs (three LEDs) are toggling well in StartDefaultTask().
I'm attaching the project (I just introduced a modification on PD12 to PD15 gpio pins to be as outputs for LEDs + Clock config to adapt it to the disco board).
PS: ST-Link Utility is a deprecated tool and no more supported. Use STM32CubeProgrammer instead.
2024-05-13 09:50 AM - edited 2024-05-13 11:54 AM
Thanks a lot for your help. I have another board, I'll try it.
So if the other board is also not working with freertos is there something else I can do?
For me it's super wired that everything is only working without RTOS.
Is there another dev board with ethernet available which is freeRTOS tested?
:(
Thanks for your help
Update: other board is also not working
Update2: I tried to flash the program without freeRTOS with STM32CubeProgrammer => working, but as soon as I enable freeRTOS the issue is back - nothing happens :(
2024-05-13 03:04 PM
That's weird! And yet I didn' change much to your code and I didn't touch to your project settings!