cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 Mcu clock setup

rohitkumarkv07
Associate III

Hello sir, I have developed MCU clock setup using two functions Mcu_init and mcu_initclock in stm32f407 board. 

Now I want to develop Distribute PLL and get PLL status. Can you help me out. 

I have attached my mcu.c here for your convinience.

#include "Mcu.h"
#include "Mcu_Config.h"
#include "Mcu_Internal.h"
#include "Mcu_RegTypes.h"

Mcu_ConfigType* Mcu_pConfigPtr = NULL_PTR;

static FUNC(void, MCU_CODE) Mcu_Pwr_Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_Flash_Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AllPeriphralReset(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AHB1Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AHB2Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AHB3Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_APB1Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_APB2Init(VAR( void, AUTOMATIC));

static FUNC(void, MCU_CODE) Mcu_Pwr_Init(VAR( void, AUTOMATIC))
{
	PwrConfigType* LpPwrConfigPtr;
	PWR_RegTypedef* LpPWR_Reg = PWR_REGADDRESS;

	LpPwrConfigPtr = Mcu_pConfigPtr->PWRConfgSet;
#if(MCU_VOS_SCALE_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.VOS;
#endif
#if(MCU_FPDS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.FPDS;
#endif
#if(MCU_DBP_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.DBP;
#endif
#if(MCU_PLS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.PLS;
#endif
#if(MCU_PVDE_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.PVDE;
#endif
#if(MCU_PDDS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.PDDS;
#endif
#if(MCU_LPDS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.LPDS;
#endif

#if(MCU_BRE_USED == STD_ON)
	LpPWR_Reg->CSR |= LpPwrConfigPtr->PwrCSRConfgVal.BRE;
#endif
#if(MCU_EWUP_USED == STD_ON)
	LpPWR_Reg->CSR |= LpPwrConfigPtr->PwrCSRConfgVal.EWUP;
#endif

}
static FUNC(void, MCU_CODE) Mcu_Flash_Init(VAR( void, AUTOMATIC))
{
	FLASHConfigType* LpFlashconfigPtr;
	FLASH_RegTypedef* LpFLASH_Reg = FLASH_REGADDRESS;
	LpFlashconfigPtr = Mcu_pConfigPtr->FlashConfgSet;
#if(MCU_DCRST_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.DCRST;
#endif
#if(MCU_ICRST_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.ICRST;
#endif
#if(MCU_LATENCY_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.LATENCY;
#endif


#if(MCU_DCEN_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.DCEN;
#endif
#if(MCU_ICEN_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.ICEN;
#endif
#if(MCU_PRFTEN_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.PRFTEN;
#endif

}
static FUNC(void, MCU_CODE) Mcu_AllPeriphralReset(VAR( void, AUTOMATIC))
{
	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	/*Reset the MCU Peripherals */
	LpRCC_Reg->AHB1RSTR =(uint32)(RCC_AHB1RSTR_RESET);
	LpRCC_Reg->AHB1RSTR =(uint32)(0x00000000);
	LpRCC_Reg->AHB2RSTR =(uint32)(RCC_AHB2RSTR_RESET);
	LpRCC_Reg->AHB2RSTR =(uint32)(0x00000000);
	LpRCC_Reg->AHB3RSTR =(uint32)(RCC_AHB3RSTR_RESET);
	LpRCC_Reg->AHB3RSTR =(uint32)(0x00000000);
	LpRCC_Reg->APB1RSTR =(uint32)(RCC_APB1RSTR_RESET);
	LpRCC_Reg->APB1RSTR =(uint32)(0x00000000);
	LpRCC_Reg->APB2RSTR =(uint32)(RCC_APB2RSTR_RESET);
	LpRCC_Reg->APB2RSTR =(uint32)(0x00000000);
	/*Reset the MCU Peripherals */
}
static FUNC(void, MCU_CODE) Mcu_AHB1Init(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;

	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;

	/*McuAHB1ENRConfgVal*/
#ifdef MCU_USB_OTG_USED
#if(OTGHSULPIEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.OTGHSULPIEN;
#endif
#if(OTGHSEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.OTGHSEN;
#endif
#endif

#ifdef MCU_ETHMAC_USED
#if(ETHMACPTPEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACPTPEN;
#endif
#if(ETHMACRXEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACRXEN;
#endif
#if(ETHMACTXEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACTXEN;
#endif
#if(ETHMACEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACEN;
#endif
#endif

#ifdef MCU_DMA_USED
#if(DMA2EN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.DMA2EN;
#endif
#if(DMA1EN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.DMA1EN;
#endif
#endif

#ifdef MCU_CCM_DATA_RAM_USED
#if(CCMDATARAMEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.CCMDATARAMEN;
#endif
#endif

#ifdef MCU_BKP_SRAM_USED
#if(BKPSRAMEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.BKPSRAMEN;
#endif
#endif

#ifdef MCU_CRC_USED
#if(CRCEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.CRCEN;
#endif
#endif

#ifdef MCU_GPIO_USED
#if(GPIOIEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOIEN;
#endif
#if(GPIOHEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOHEN;
#endif
#if(GPIOGEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOGEN;
#endif
#if(GPIOFEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOFEN;
#endif
#if(GPIOEEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOEEN;
#endif

#if(GPIODEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIODEN;
#endif

#if(GPIOCEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOCEN;
#endif
#if(GPIOBEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOBEN;
#endif
#if(GPIOAEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOAEN;
#endif
#endif
}
static FUNC(void, MCU_CODE) Mcu_AHB2Init(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;

	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;

    /*McuAHB2ENRConfgVal*/
#if(OTGFSEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.OTGFSEN;
#endif
#if(RNGEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.RNGEN;
#endif
#if(HASHEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.HASHEN;
#endif
#if(CRYPEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.CRYPEN;
#endif
#if(DCMIEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.DCMIEN;
#endif


}
static FUNC(void, MCU_CODE) Mcu_AHB3Init(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;

	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;

	/*McuAHB3ENRConfgVal*/
#if(DCMIEN_USED == STD_ON)
	LpRCC_Reg->AHB3ENR |= LpMcuClockConfigPtr->McuAHB3ENRConfgVal.FSMCEN;
#endif
}
static FUNC(void, MCU_CODE) Mcu_APB1Init(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;

	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;


	/*McuAPB1ENRConfgVal*/
#ifdef MCU_DAC_USED
#if(DACEN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.DACEN;
#endif
#endif
#ifdef MCU_PWR_USED
#if(PWREN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.PWREN;
#endif
#endif
#ifdef MCU_CAN_USED
#if(CAN2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.CAN2EN;
#endif
#if(CAN1EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.CAN1EN;
#endif
#endif

#ifdef MCU_I2C_USED
#if(I2C3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.I2C3EN;
#endif
#if(I2C2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.I2C2EN;
#endif
#if(I2C1EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.I2C1EN;
#endif
#endif
#ifdef MCU_UART_USED
#if(UART5EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.UART5EN;
#endif
#if(UART4EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.UART4EN;
#endif
#endif
#ifdef MCU_USART_USED
#if(USART3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.USART3EN;
#endif
#if(USART2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.USART2EN;
#endif
#endif
#ifdef MCU_SPI_USED
#if(SPI3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.SPI3EN;
#endif
#if(SPI2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.SPI2EN;
#endif
#endif
#if(WWDGEN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.WWDGEN;
#endif
#ifdef MCU_TIM_USED
#if(TIM14EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.UART4EN;
#endif
#if(TIM13EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM13EN;
#endif
#if(TIM12EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM12EN;
#endif
#if(TIM7EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM7EN;
#endif
#if(TIM6EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM6EN;
#endif
#if(TIM5EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM5EN;
#endif
#if(TIM4EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM4EN;
#endif
#if(TIM3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM3EN;
#endif
#if(TIM2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM2EN;
#endif
#endif

}
static FUNC(void, MCU_CODE) Mcu_APB2Init(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;

	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;


	/*McuAPB2ENRConfgVal*/
#ifdef MCU_TIM_USED
#if(TIM11EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM11EN;
#endif
#if(TIM10EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM10EN;
#endif
#if(TIM9EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM9EN;
#endif
#endif
#if(SYSCFGEN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.SYSCFGEN;
#endif
#if(SPI1EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.SPI1EN;
#endif
#if(SPI1EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.SDIOEN;
#endif
#ifdef MCU_ADC_USED
#if(ADC3EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.ADC3EN;
#endif
#if(ADC3EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.ADC2EN;
#endif
#if(ADC3EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.ADC1EN;
#endif
#endif
#ifdef MCU_USART_USED
#if(USART6EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.USART6EN;
#endif
#if(USART5EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.USART1EN;
#endif
#endif
#ifdef MCU_TIM_USED
#if(TIM8EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM8EN;
#endif
#if(TIM1EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM1EN;
#endif
#endif
}

FUNC(void, MCU_CODE) Mcu_Init( Mcu_ConfigType* pConfigPtr)
{
	Mcu_pConfigPtr = pConfigPtr;

	Mcu_AllPeriphralReset();
	Mcu_Pwr_Init();
	Mcu_Flash_Init();
	Mcu_AHB1Init();
	Mcu_AHB2Init();
	Mcu_AHB3Init();
	Mcu_APB1Init();
	Mcu_APB2Init();
}

FUNC( Std_ReturnType, MCU_CODE) Mcu_InitClock( VAR( uint8, AUTOMATIC) ClockSetting)
{
	McuClockConfigType* LpMcuClockConfigPtr;
	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;
	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;



#if(MCU_PLLI2S_USED == STD_ON)
    LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.PLLI2SON;
#endif
#if(MCU_PLL_USED == STD_ON)
    LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.PLLON;
#endif
#if(MCU_CSS_USED == STD_ON)
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.CSSON;
#endif

#if(MCU_HSEBYP_USED == STD_ON)
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.HSEBYP;
#endif

#if(MCU_HSE_USED == STD_ON)
    LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.HSEON;
#endif

#if(MCU_HSITRIM_USED == STD_ON)
    LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.HSITRIM;
#endif

#if(MCU_HSI_USED == STD_ON)
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.HSION;
#endif


#if(MCU_PLLM_USED == STD_ON)
	LpRCC_Reg->PLLCFGR |= LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLM;
#endif
#if(MCU_PLLN_USED == STD_ON)
	LpRCC_Reg->PLLCFGR |= LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLN;
#endif
#if(MCU_PLLP_USED == STD_ON)
	LpRCC_Reg->PLLCFGR |= LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLP;
#endif
#if(MCU_PLLSRC_HSE_USED == STD_ON)
	LpRCC_Reg->PLLCFGR |= LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLSRC;
#endif
#if(MCU_PLLQ_USED == STD_ON)
	LpRCC_Reg->PLLCFGR |= LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLQ;
#endif


#if(MCU_PRE2_AHB_2_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.HPRE;
#endif
#if(MCU_PRE1_AHB_4_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.PPRE1;
#endif
#if(MCU_HRPE_SYSCLK_1_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.PPRE2;
#endif
#if(MCU_SW_PLL_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.SW;
#endif
#if(MCU_MCO2_SYSCLK_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO2;
#endif
#if(MCU_MCO2PRE_2_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO2PRE;
#endif
#if(MCU_MCO1PRE_2_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO1PRE;
#endif
#if(MCU_I2SSRC_PLL_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.I2SSRC;
#endif
#if(MCU_MCO1_HSE_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO1;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.RTCPRE;
#endif


#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.PLLI2SRDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.PLLRDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.HSERDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.HSIRDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.LSERDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.LSIRDYIE;
#endif


#if 0
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.BDRST;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.RTCEN;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.RTCSEL;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.LSEBYP;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.LSEON;
	LpRCC_Reg->CSR = LpMcuClockConfigPtr->McuCSRConfgVal.LSION;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.SSCGEN;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.SPREADSEL;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.INCSTEP;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.MODPER;
	LpRCC_Reg->PLLI2SCFGR = LpMcuClockConfigPtr->McuPLLI2SCFGRConfgVal.PLLI2SR;
	LpRCC_Reg->PLLI2SCFGR = LpMcuClockConfigPtr->McuPLLI2SCFGRConfgVal.PLLI2SN;
#endif
	return E_OK;
}
/*
FUNC(Mcu_ResetType, MCU_CODE) Mcu_GetResetReason(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;
	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;
	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;

	VAR(Mcu_ResetType, AUTOMATIC) eResetReason;
    eResetReason = (uint32)LpRCC_Reg->CSR;

    return (Mcu_ResetType)eResetReason;

}*/




 

#include "Mcu.h"
//#include"stm32f407xx.h"
#include "stm32f4xx.h"
#include "Mcu_RegTypes.h"
#include"Mcu_InternalTypes.h"
#define LED_PIN 12  // Assuming the LED is connected to GPIO Port D, Pin 13

void delay(uint32_t time) {
    while(time--);
}

int main()
{
	Mcu_Init(&Mcu_ConfigSet[0]);
	Mcu_InitClock(0);


	// Enable the clock for GPIO Port D using AHB1 peripheral clock enable register
	    //RCC->AHB1ENR |= RCC_AHB1ENR_GPIODEN;

	    // Configure PD12 as output
	    GPIOD->MODER |= GPIO_MODER_MODER12_0;

	while(1)
	{
		 // Turn on the LED (set PD12 high)
		        GPIOD->ODR |= GPIO_ODR_ODR_12;

		        // Delay
		        delay(500000);

		        // Turn off the LED (set PD12 low)
		        GPIOD->ODR &= ~GPIO_ODR_ODR_12;

		        // Delay
		        delay(500000);
	}
}

 

7 REPLIES 7
Andrew Neil
Evangelist III

So is your other problem now resolved:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/stm32f407-clock-setup-using-registers/td-p/663048

If so, please mark the solution in that thread.

rohitkumarkv07
Associate III

Help me in this.

You've marked this as solved!

🤔

rohitkumarkv07
Associate III

no my issue is not solved

So why did you mark it as solved, then?

rohitkumarkv07
Associate III

It's by mistake

Andrew Neil
Evangelist III

This seems to be the same as your previous post:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/stm32f407-clock-setup-using-registers/td-p/663048 

So, again, why not create a working setup using CubeMX - then take the required settings from that?

Then debug your code against the Cube code.