2020-11-10 10:12 PM
Hi I am working on a small project where I need to sample couple of ADC channels.
I am using STM32F405RG. ADC1 is running in continuous and scan mode with DMA. I am using ping pong buffers to send ADC data through USART.
After gathering some data I plot them in MATLAB.
Problem is that there are random spikes in my ADC values an example is shown below.
X axis is Seconds, Y axis is voltage. Graph belongs to an ADC channel where approximately 2.6 volts needs to be read.
Has anyone encountered this ?
2020-11-16 6:01 AM
It's going to be an issue of having grounds which are separated by a potential. Typically this is solved by having a solid ground plane and tying ground pins to it with vias very close to the pin.
Is this a custom board? What does your layout look like? What else is connected to the same power/ground rails?
2020-11-16 1:06 PM
The first think is - you have to have straight line @ 0V when you put ground directly on ADC pin. The spikes comes from your ADC wiring, without drawing and picture of it, it is just guessing work.
2020-11-16 2:34 PM
ST has AN2834 and AN4073 as guidelines to the ADC.
JW