cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8T6 Failed in immunity test at 475 MHz frequency. what are precaution for STM32F103 Microcontroller to success the EMC test?

Deepak.Aagri
Associate III

STM32103C8T6 face the system reset during the immunity test at 470Mhz 10V/meter of EN 50130-4:2011 standards.

2 REPLIES 2
SBEN .2
Senior II

Hello @Deepak.Aagri​ ,

Generally speaking, the first thing I'd think of is shielding the microcontroller and its satellite components (XTAL, decoupling capacitors, etc...). Otherwise, check this document: EMC design guide for STM8, STM32 and Legacy MCUs - Application note

Best regards,

@SBEN .2​ 

Deepak.Aagri
Associate III

Thanks ... Please provide the vender details to order 250 number of shields for ST microcontroller ....