2021-07-07 12:04 AM
Hi,
i am trying to implement a SPI communication with STM32H7(Master) to STM32F1(slave) with interrupt mode. In Slave Side SPI3(with NSS Hardware Input) i have enabled, In Master Side SPI6 (GPIO Pin Toggling for SS) I have Enabled
My Issue is at Slave Side I have this Function to receive from master HAL_SPI_Receive_IT(&hspi3, RX_Buffer, 4); and Its not Entering into -> void SPI3_IRQHandler(void) function. How we can resolve this issue? and Only one time below condition gets satisfied in HAL_SPI_Receive_IT function
"if (hspi->State != HAL_SPI_STATE_READY)"
2021-07-07 2:43 AM
Hello,
Does RXNE flag is set even if you don't have the interrupt ? Are you sure your SPI slave is ready before the master. Because, for instance, if you sent one data from the master, the SPI clock starts and the data is transferred to the slave. But if this one is enabled somewhere after the clock has already started from the master, the slave is waiting for missing clock to set RXNE flag at 1.
So Slave needs always to be ready before the master.
BR
2021-07-07 3:22 AM
Dear CPINA,
Yes, After SPI3_Init() function i am enabling RSNE flag "__HAL_SPI_ENABLE_IT(&hspi3, SPI_IT_RXNE);" and also setting DFF bit and SPE bit
"hspi3.Instance->CR1 = 0x0840;"
But Once "HAL_SPI_Receive_IT(&hspi3,(uint8_t*)&read,4);" this function get completed in CR2 Register ERRIE Bit also has been set
Can you please help me of this configuration sequence!
Thanks
2021-07-07 3:24 AM
Dear CPINA,
Could you please help (Please Find the Below Comment)
2021-07-07 6:48 AM
Did you enable the NVIC interrupt?
2021-07-07 7:15 AM
as said by @TDK , Can you check that you enabled the NVIC Interrupt. The ERROR you get are probably linked to overrun (you can check the flag OVR) because your data is accumulated without being read by your software from the interrupt which is not generated.
2021-07-10 4:50 AM
Hi
Yes i have enabled both side(master and slave) interrupt, i did a mistake in clock settings that i have resolved now now i am able to receive the data from master side but only one byte alone receiving
Master Side in While(1) loop :
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_Delay(10);
HAL_SPI_Transmit_IT(&hspi6, TX_Buffer, 3);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
Slave side:
/* USER CODE BEGIN 2 */
hspi3.Instance->CR1 = 0x0840;
HAL_SPI_Receive_IT(&hspi3,(uint8_t*)&read,3);
and in Interrupt Handler
RX_Resp_Buffer[i++] = hspi3.Instance->DR;
Did i miss Something? or anything i need to change
2021-07-10 5:21 AM
HAL_SPI_Transmit_IT is asynchronous. You need to wait for the transfer to complete before raising the CS line.
HAL_SPI_Receive_IT will put data into the buffer, you shouldn't read it from DR, you should read it from the buffer. ("read" in this case)
> hspi3.Instance->CR1 = 0x0840;
Not sure what this does offhand but you generally shouldn't be messing with registers if you're using regular HAL functions.
2021-07-13 12:04 AM
Dear TDK,
I have tested the way that you have mentioned
Master side :
uint8_t TX_Buffer[2] = {9,7};
while(1)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_Delay(10);
HAL_SPI_Transmit_IT(&hspi6, TX_Buffer, 2);
HAL_Delay(500);
if(SPI_FLAG_EOT)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
}
}
Slave side:
while(1)
{
HAL_SPI_Receive_IT(&hspi3,(uint8_t*)&read,2);
}
As you said in this case read buffer is not receiving anything in by reading from DR register in spi3_irqHandler function only i can read only one data Can you please help me?
2021-07-13 7:24 AM
There are a lot of issues with this code.
I suggest following an example from CubeMX:
Additionally, I would monitor the return value from HAL_SPI_* calls and output debug information if it's not HAL_OK so that you can fix your program.
Don't call HAL_SPI_Transmit_IT/HAL_SPI_Receive_IT repeatedly. Wait for it to complete the transaction before calling it again.
Note that if(SPI_FLAG_EOT) always returns true since SPI_FLAG_EOT is nonzero. If you're trying to test for completion, check the state of the peripheral within the hspi6 handle instead.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.