2025-01-08 1:59 AM - last edited on 2025-01-08 2:08 AM by Andrew Neil
Hello everyone,
I would like to know the technology node (i.e. 180nm, 90nm, etc.) of the STM32 microcontroller STM32F103C8T6. I can not find this information.
Thanks in advance.
Best regards.
Marco
Solved! Go to Solution.
2025-01-08 3:34 AM
Yes, the original STM32F103 from STMicroelectronics is produced in 180nm technology.
However, we cannot comment on illegal counterfeits, which are particularly often seen with the STM32F103C8T6 (e.g. on the so-called Blue Pill). In such a case, you must contact the counterfeiter in question.
Regards
/Peter
2025-01-08 2:14 AM
As far as I know STM32F1 is 180nm technology.
2025-01-08 3:34 AM
Yes, the original STM32F103 from STMicroelectronics is produced in 180nm technology.
However, we cannot comment on illegal counterfeits, which are particularly often seen with the STM32F103C8T6 (e.g. on the so-called Blue Pill). In such a case, you must contact the counterfeiter in question.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.