cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx Feature request : remove the dialog after code generation

JulienD
Senior
Posted on May 09, 2015 at 19:35

Hi,

This dialog is pretty usefull the first time and pretty useless all the others.

If there's a better place to put feature request, please tell, I will do it.

Regards

Julien

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on May 19, 2015 at 18:29

Hi Julien,

Could you please tell me about which ''dialog'' are you speaking? Sorry, it is not clear.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

JulienD
Senior
Posted on May 25, 2015 at 11:28

Hi Mayla,

Yes, sure.

Just after menu ''code generate'' click OK.

Dialog is '' the code is successfully generated under xxx.  open folder / open project / close.

Instead of removing, it can be a checkbox ''do not show in future'' or any other good idea...

Have a nice day.

Julien

Katzenberger.Michael
Associate III
Posted on November 20, 2016 at 12:54

Yes, I definitely vote for this feature request !

Best regards,

Michael.