2024-06-21 1:38 PM
Hi,
We were using CubeProgrammer on Windows to program our MCU in DFU mode and everything was moving well until we noticed MAC does not detect USB in DFU mode.
So, I am wondering if there is something we are missing to do which the MAC operating system does not detect STM32 in DFU mode. Is it a driver or MAC support?
Looking forward for your help as we and our customers are really in need of using the DFU. Should you need more information, I can send you screen shots.
Thanks
Would appreciate @Houda GHABRI @Ben K helps if you can comment based on recent posts I see in other forum posts.
2024-06-22 11:06 AM
Dear @ashah.16 ,
can you tell us what is the exact device and if using the internal bootloader DFU or a customer IAP DFU . If the same hardware is working on Windows, it might be a driver problem or a timing issue . Is that possible to put a USB hub between the MAC and the device and see if it works ?
Ciao
STOne-32