2023-02-01 12:28 AM
2023-02-01 1:35 AM
Hello @Andreas Bolsch,
The issue is confirmed and it will be changed on the next document revision.
For the RCC_CR, the HSIDIV and HSIKER DIV reset value are missing, but they are indicated in the bitfield explanation.
For the IDCODE it is wrong on the introduction of the part 26.5.3 (0x0BB11477 is the cortex M0 ID code) but good in the table 123.
I reported internally.
Internal ticket number: 144181 (This is an internal tracking number and is not accessible or usable by customers).
Best regards,
Simon
2023-02-01 12:37 AM
Hello @Andreas Bolsch
Thanks for sharing this issue.
I will check this and take the necessary action.
Imen
2023-02-01 1:35 AM
Hello @Andreas Bolsch,
The issue is confirmed and it will be changed on the next document revision.
For the RCC_CR, the HSIDIV and HSIKER DIV reset value are missing, but they are indicated in the bitfield explanation.
For the IDCODE it is wrong on the introduction of the part 26.5.3 (0x0BB11477 is the cortex M0 ID code) but good in the table 123.
I reported internally.
Internal ticket number: 144181 (This is an internal tracking number and is not accessible or usable by customers).
Best regards,
Simon