cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C0 Can not Connect STMStudio After Upload Code

Embedded_Class
Associate

Hi Community,
I’m having an issue with connecting the STMStudio application.
When I plug the programmer USB into the computer, the connection works without any problems. However, if I upload code via Keil uVision, I am unable to reconnect to the STMStudio app unless I unplug and replug the USB.

My Keil Setup like is Below.

Embedded_Class_0-1735306833883.png

And My Programmer Connection

Embedded_Class_1-1735306908577.png

 

Is there any point that ı can not catch?

Thanks for supporters.

 

 

1 REPLY 1
Imen.D
ST Employee

Hello @Embedded_Class ,

What exactly did the error message say?

If possible, please post the log file (error.log) that should be into Program Files (x86)/STMicroelectronics/STMStudio/dll 

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen