2024-12-27 5:57 AM
Hi Community,
I’m having an issue with connecting the STMStudio application.
When I plug the programmer USB into the computer, the connection works without any problems. However, if I upload code via Keil uVision, I am unable to reconnect to the STMStudio app unless I unplug and replug the USB.
My Keil Setup like is Below.
And My Programmer Connection
Is there any point that ı can not catch?
Thanks for supporters.
2025-01-02 1:44 AM
Hello @Embedded_Class ,
What exactly did the error message say?
If possible, please post the log file (error.log) that should be into Program Files (x86)/STMicroelectronics/STMStudio/dll