2017-06-18 12:21 AM
Hello i have a program on the 32F030f4p6 chip for testing the system clock frequency. It blinks an LED at about 1Hz. the problem is that when i change the PLL multiplier from 2 to 12 the LED still blinks at the same 1Hz. i configured the system clock for 48MHz but it seems to be running at 8MHz. i don't know what i'm doing wrong.
#include 'stm32f030x4.h'
int main(void)
{
// sysclock configuration
RCC->CR |= RCC_CR_HSION; // 8MHz
RCC->CR |= RCC_CR_PLLON;
RCC->CFGR &= ~RCC_CFGR_PLLSRC;
RCC->CFGR |= RCC_CFGR_PLLSRC_HSI_DIV2; // PLL source = 4MHz
RCC->CFGR &= ~RCC_CFGR_PLLMUL;
RCC->CFGR |= RCC_CFGR_PLLMUL12; // <-- changing the multiplier has no effect on LED frequency
RCC->CFGR &= ~RCC_CFGR_SW;
RCC->CFGR |= RCC_CFGR_SW_PLL; // PLL selected as system clock
RCC->CFGR &= ~RCC_CFGR_HPRE;
RCC->CFGR |= RCC_CFGR_HPRE_DIV1; // ahbclk not divided
RCC->CFGR &= ~RCC_CFGR_PPRE;
RCC->CFGR &= RCC_CFGR_PPRE_DIV1; // apbclk not divided
RCC->AHBENR |= RCC_AHBENR_GPIOAEN;
// GPIO pin configuration
pinpos = 4;
GPIOA->OSPEEDR &= ~(GPIO_OSPEEDR_OSPEEDR0 << (pinpos * 2));
GPIOA->OSPEEDR |= ((uint32_t)(0x03) << (pinpos * 2)); // high speed 50MHz
GPIOA->OTYPER &= ~((GPIO_OTYPER_OT_0) << ((uint16_t)pinpos));
GPIOA->OTYPER |= (uint16_t)(((uint16_t)0x00) << ((uint16_t)pinpos)); // type push/pull
GPIOA->MODER &= ~(GPIO_MODER_MODER0 << (pinpos * 2));
GPIOA->MODER |= (((uint32_t)0x01) << (pinpos * 2)); // mode = output
GPIOA->PUPDR &= ~(GPIO_PUPDR_PUPDR0 << ((uint16_t)pinpos * 2));
GPIOA->PUPDR |= (((uint32_t)0x00) << (pinpos * 2)); // no pull up or down
while(1){
GPIOA->ODR ^= (1 << 4); // toggle LED
for (y = 0; y<500; y++){ // delay about 1 second
for (x = 0; x<500; x++){}
}
}
}
#stm-32f030f4p6-pll-configuration
Solved! Go to Solution.
2017-06-18 02:13 AM
You cannot switch PLL multiplier while PLL is on, and you have to wait until PLL locks after switching it on, before using as a system clock.
See the PLL configuration modification code example in appendix A in RM.
Also note, that FLASH latency has to be set properly prior switching to a higher system clock, if running from FLASH.
JW
2017-06-18 02:13 AM
You cannot switch PLL multiplier while PLL is on, and you have to wait until PLL locks after switching it on, before using as a system clock.
See the PLL configuration modification code example in appendix A in RM.
Also note, that FLASH latency has to be set properly prior switching to a higher system clock, if running from FLASH.
JW
2017-06-18 04:53 PM
much obliged now i got it goin on :-)
2017-06-19 06:40 AM
Hi Mike,
Happy that your issue is solved .
Could you please mark the question as answered. This will help to m
inimize the duplication of subjects treating issues already solved.
https://community.st.com/0D50X00009bMM5DSAW
Khouloud.
2020-06-23 01:34 PM
Your note about FLASH latency... Saved my day. I was about to go crazy. Thanks.