2017-04-27 5:46 AM
Hi everyone,
I turn to you in complete despair. I thought I would start tonight with My Nucleo, but couldn't even get past the Installation of the CubeMX software. When I double click on the app (SetupSTM32CubeMX-4.20.1) or open it via left click and open, I get the message:
“SetupSTM32CubeMX-4.20.1� is an application downloaded from the Internet. Are you sure you want to open it?'
as usual. But after clicking on open, nothing happens. I also tried to execute it via terminal as suggested by another post, but get:
Jean-Marcs-MacBook-Pro-2:A Joeme$ java -jar SetupSTM32CubeMX-4.20.1.app
Invalid or corrupt jarfile SetupSTM32CubeMX-4.20.1.app
Does someone know how to solve this? Thank you in advance!
Solved! Go to Solution.
2017-04-28 10:19 AM
the mac installer is broken and has been for many versions.
dont try to launch the .app, launch the .exe with the java -jar command. you will also need to use sudo to do it because it installs in the applications folder
2017-04-27 9:59 AM
Hi,
Are you following the instructions in this
manual to install STM32CubeMX in command-line mode and install the software requirements as Java Development Kit 1.7.0_45 ?You should make sure that you have administrator rights.
2017-04-27 8:51 PM
You may want to update Java.
Also, try downloading again, your file may be corrupted.
2017-04-28 10:19 AM
the mac installer is broken and has been for many versions.
dont try to launch the .app, launch the .exe with the java -jar command. you will also need to use sudo to do it because it installs in the applications folder