2024-09-10 03:51 AM
Hi All,
I am currently working on the CAN normal mode in a custom board with MCU STM32F098RCT6 and CAN transceiver TJA1042. Very first I tried the loopback mode and it was successful. Then I am now trying to interface two custom boards using the normal mode. But there is no output.
Please give some insight about this.
Here is the code:
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan;
/* USER CODE BEGIN PV */
CAN_TxHeaderTypeDef TxHeader;
CAN_RxHeaderTypeDef RxHeader;
uint8_t TxData[2];
uint8_t RxData[2];
uint32_t TxMailbox;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_CAN_Init(void);
/* USER CODE BEGIN PFP */
HAL_StatusTypeDef CAN_Polling(void);
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CAN_Init();
/* USER CODE BEGIN 2 */
if(CAN_Polling() != HAL_OK){
while(1){}
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_11);
HAL_Delay(500);
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief CAN Initialization Function
* @PAram None
* @retval None
*/
static void MX_CAN_Init(void)
{
/* USER CODE BEGIN CAN_Init 0 */
/* USER CODE END CAN_Init 0 */
/* USER CODE BEGIN CAN_Init 1 */
/* USER CODE END CAN_Init 1 */
hcan.Instance = CAN;
hcan.Init.Prescaler = 16;
hcan.Init.Mode = CAN_MODE_LOOPBACK;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_1TQ;
hcan.Init.TimeSeg2 = CAN_BS2_1TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = DISABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = ENABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN_Init 2 */
/* USER CODE END CAN_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_11, GPIO_PIN_RESET);
/*Configure GPIO pin : PC11 */
GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
HAL_StatusTypeDef CAN_Polling(void){
CAN_FilterTypeDef sFilterconfig;
sFilterconfig.FilterBank = 0;
sFilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterconfig.FilterIdHigh = 0x0000;
sFilterconfig.FilterIdLow = 0x0000;
sFilterconfig.FilterMaskIdHigh = 0x0000;
sFilterconfig.FilterMaskIdLow = 0x0000;
sFilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0 ;
sFilterconfig.FilterActivation = CAN_FILTER_ENABLE;
sFilterconfig.SlaveStartFilterBank = 14;
if(HAL_CAN_ConfigFilter(&hcan, &sFilterconfig) != HAL_OK)
{
Error_Handler();
}
if(HAL_CAN_Start(&hcan) != HAL_OK)
{
Error_Handler();
}
TxHeader.IDE = CAN_ID_STD;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.StdId = 0x11;
TxHeader.DLC = 2;
TxHeader.TransmitGlobalTime = DISABLE;
TxData[0] = 0xCA;
TxData[1] = 0xFE;
if( HAL_CAN_AddTxMessage(&hcan, &TxHeader, TxData, &TxMailbox) != HAL_OK)
{
Error_Handler();
}
while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan) != HAL_OK){}
if(HAL_CAN_GetRxFifoFillLevel(&hcan, CAN_RX_FIFO0) != HAL_OK)
{
Error_Handler();
}
if(HAL_CAN_GetRxMessage(&hcan, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
Error_Handler();
}
return HAL_OK;
}
Solved! Go to Solution.
2024-09-11 05:58 AM
2024-09-11 06:26 AM
Not sure how useful this will be for you, but ControllersTech did an excellent video on CAN normal mode.
2024-09-11 06:41 AM
In your code, you send and receive once in polling mode. So I don't know how you test that and what you expect as a behavior.
if( HAL_CAN_AddTxMessage(&hcan, &TxHeader, TxData, &TxMailbox) != HAL_OK)
{
Error_Handler();
}
while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan) != HAL_OK){}
if(HAL_CAN_GetRxFifoFillLevel(&hcan, CAN_RX_FIFO0) != HAL_OK)
{
Error_Handler();
}
if(HAL_CAN_GetRxMessage(&hcan, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
Error_Handler();
}
I modified your project (in attachement) to work in RX FIFO interrupt mode. SystemClock at 48MHz / CAN bitrate at 500kb/s (modified the prescaler, BS1 and BS2 with recommended values).
Unfortunately I don't have a board to test that MCU part number. So you need to test it from your side: in the Live Expression check RxData[].
Hope it helps.
2024-09-11 07:05 AM
The circuit on CAN_STBY is putting the TJA1042BT probably in standby. The STB pin is a digital input, so setting it to 1.6V is definitively not a good idea. Please remove R5 to enable the Driver.
Martin
2024-09-11 07:59 AM
@MHoll.2 wrote:
The circuit on CAN_STBY is putting the TJA1042BT probably in standby. The STB pin is a digital input, so setting it to 1.6V is definitively not a good idea. Please remove R5 to enable the Driver.
Martin
Yes it could be related to this.
2024-09-11 10:42 PM
Hi,
I tried the interrupt code you have provided. But there is no change. Nothing is receiving as RxData.
2024-09-11 10:43 PM
Hi,
thankyou for replying.
I am already using Controllers Tech video as a reference.
2024-09-11 10:51 PM - edited 2024-09-16 08:13 AM
Check your hardware. You need to check all the HW part of the CAN network. The power, the connections, the termination resistors.
You need to probe CAN_Tx and CAN_Rx pins and see what happens.