cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Bootloader Pin Availability

NAbun.1
Associate II

Hello,

I am reading AN2606 and I am wondering if I am interpreting the document correctly. Is table 113 suggesting that the FDCAN bootloader is only available on pins PH13 & PH14 in the STM32H75 series? Since these pins do not exist on the 100 pin packages of the part, is it not possible to use the FDCAN bootloader on 100 pin packages?

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Correct and correct.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

Correct and correct.

If you feel a post has answered your question, please click "Accept as Solution".
STTwo-32
ST Employee

Hello @NAbun.1 

As said @TDK , Booth LQFP100 and LQFP144 does not support the FDCAN bootloader.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.