Skip to main content
Tobe
Senior III
September 16, 2024
Question

Startup time of NUCLEO G431RB varies greatly

  • September 16, 2024
  • 2 replies
  • 705 views

After troubleshooting this issue , i found, that i have a greatly varying startup time.

I have this minimal code:

int main(void)
{
	/* GPIO Ports Clock Enable */
	__HAL_RCC_GPIOC_CLK_ENABLE();

	GPIO_InitTypeDef my_GPIO_InitStruct = {0};

	// TEST PIN
	my_GPIO_InitStruct.Pin = GPIO_PIN_3;
	my_GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	my_GPIO_InitStruct.Pull = GPIO_PULLUP;
	HAL_GPIO_Init(GPIOC, &my_GPIO_InitStruct);

	GPIOC->BSRR = (uint32_t) GPIO_PIN_3;
}

 I know that some clock setting needs some time, but this? it varies from 100ms to 1600ms !

Could it be, that the chip is bad?

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
September 16, 2024

You haven't shown what your clock setup is.

How are you measuring the startup time?

Does it make any difference if the startup is from a power cycle, or just a reset?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tobe
TobeAuthor
Senior III
September 16, 2024

I removed my clock setup to create a minimal code. See the picture for the measurement. I do reset with a wavegen.

I also measured with power cycle: With powercycle it was very constant (2.143s).

But now that i switched back, i can not reproduce this issue anymore. Maybe i got the setup not back as it was with the issue? Or maybe a powercycle removed the issue.

 

It is not constant at about 200us.