2020-04-07 6:06 AM
Pardon me for asking repeated questions on SPI, but it's giving me a lot of issues. So far I have configured two STM32 boards as master and slave, and ran code for MOSI and MISO lines individually which seemed to work fine. Now that I combine those codes for full duplex communication, I am getting wrong data.
Assume all functions called work correctly.
Master code :
#include "stm32l4xx.h" // Device header
#include <string.h>
#define CS_LOW (GPIOA->BSRR = (1<<20))
#define CS_HI (GPIOA->BSRR = (1<<4))
void SPI_init(void);
void SPI_write(uint8_t data);
void SPI_writestring(char* str);
void delayms(int count);
void setclkfreq(void);
void UART_init(void);
void uart_txchar(char c);
void uart_txstr(char* string);
int main()
{
char buff[16] = {0};
setclkfreq(); //set clock to 16Mhz
SPI_init();
UART_init();
CS_HI;
while(1)
{
//MOSI
CS_LOW;
SPI_writestring("Execute");
CS_HI;
delayms(1);
//*********************************************************
//MISO
CS_LOW;
for(int i=0; i<12; i++)
{
SPI_write(0x00); //write dummy byte
buff[i] = *(__IO uint8_t *)&SPI1->DR; //store MISO data in buff
}
CS_HI;
uart_txstr(buff);
uart_txstr("\n\r");
delayms(500);
}
}
void SPI_init(void)
{
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN;
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN;
GPIOA->MODER &=~(3<<8 | 3<<10 | 3<<12 | 3<<14);
GPIOA->MODER |= (1<<8 | 2<<10 | 2<<12 | 2<<14); //CS is selected as GPO while others are AFs
//GPIOA->PUPDR |= 1<<12; //pull up MISO line
GPIOA->AFR[0] &=~(0XF<<20 | 0xF<<24 | 0xF<<28);
GPIOA->AFR[0] |= (5<<20 | 5<<24 | 5<<28); //af for mosi,miso and sck
SPI1->CR1 &=~ (SPI_CR1_SPE);
SPI1->CR1 |= (3<<3) | SPI_CR1_MSTR | SPI_CR1_SSI | SPI_CR1_SSM;
SPI1->CR1 |= SPI_CR1_SPE;
}
void SPI_write(uint8_t data)
{
*(__IO uint8_t *)&SPI1->DR = data;
while(!(SPI1->SR & SPI_SR_TXE));
while((SPI1->SR & SPI_SR_BSY));
}
void SPI_writestring(char* str)
{
int len = strlen(str);
for(int i=0; i<len; i++)
{
//CS_LOW;
SPI_write(str[i]);
//CS_HI;
}
}
void delayms(int count)
{
int i;
SysTick->LOAD = 16000; //16000 cycles in 1 ms
SysTick->VAL = 0; //reset current value to 0
SysTick->CTRL = 5; //clksource = internal. counter enabled. interrupt disabled
for(i=0; i<count; i++) //repeat 1ms cycles count number of times
{
while((SysTick->CTRL & 0x10000)==0){} //do nothing till Countflag becomes 1
}
SysTick->CTRL=0; //disable counter
}
void setclkfreq(void)
{
FLASH->ACR &=~ FLASH_ACR_LATENCY;
FLASH->ACR |= FLASH_ACR_LATENCY_0WS;
RCC->CR |= RCC_CR_MSION; //turn on MSI (Multi Speed Internal)
RCC->CFGR &=~ RCC_CFGR_SW;
while(!(RCC->CR & RCC_CR_MSIRDY));
RCC->CR &=~ RCC_CR_MSIRANGE;
RCC->CR |= RCC_CR_MSIRANGE_8; //16Mhz
RCC->CR |= RCC_CR_MSIRGSEL;
while(!(RCC->CR & RCC_CR_MSIRDY));
}
void UART_init(void)
{
RCC->APB1ENR1 &=~ RCC_APB1ENR1_USART2EN;
RCC->APB1ENR1 |= RCC_APB1ENR1_USART2EN; //ENABLE UART2
RCC->AHB2ENR &=~ RCC_AHB2ENR_GPIOAEN;
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN; //PORT A enable
GPIOA->AFR[0] &=~ 0XF00;
GPIOA->AFR[0] |= 0X700; //ENABLE transmit
GPIOA->MODER &=~(3<<4);
GPIOA->MODER |= 2<<4; //PA2 output
USART2->CR1 &=~ (USART_CR1_UE);
USART2->BRR = 0x683; // 9600 bps
USART2->CR1 |= USART_CR1_TE;
USART2->CR1 |= USART_CR1_UE;
}
void uart_txchar(char c)
{
while(!(USART2->ISR & (USART_ISR_TXE)));
USART2->TDR = c;
while(!(USART2->ISR & USART_ISR_TC));
}
void uart_txstr(char* string)
{
while(*string)
{
uart_txchar(*(string++));
}
}
Slave side code:
#include "stm32f4xx.h" // Device header
#include <string.h>
/*
PA5 - SCK
PA4 - NSS
PA7 -MOSI
PA6 - MISO
*/
#define CS_HI (GPIOA->ODR |= 1<<4)
#define CS_LOW (GPIOA->ODR &=~(1<<4))
void SPI1_init(void);
char SPI_read(void);
void delayms(int count);
void uart_txchar(char c);
char uart_rx(void);
void UART_init(void);
void uart_txstr(char* string);
void SPI_write(char data);
void SPI_writestring(char* str);
int main()
{
char buff[16] = {0};
char c;
UART_init();
SPI1_init();
while(1)
{
//MOSI
uart_txstr("\n\rReceived : ");
for(int i=0; i<7; i++)
{
buff[i] = SPI_read();
}
uart_txstr(buff);
delayms(1);
//***********************************************************
//MISO
SPI_writestring("Acknowledged");
delayms(500);
}
}
void SPI1_init(void)
{
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; //enable clock to PortA
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; //enable clock to SPI1
GPIOA->MODER &= ~(3<<14 | 3<<10 | 3<<12 | 3<<8); //clear SPI bits
GPIOA->MODER |= (2<<10 | 2<<14 | 2<<12 | 2<<8 ); //set MOSI,MISO,NSS,SCK bits for AF
GPIOA->PUPDR |= 1<<14;
//GPIOA->PUPDR |= 2<<12; //pull down miso
GPIOA->AFR[0] &= ~(0xF<<16 | 0xF<<20 | 0xF<<24 | 0xF<<28); //clear AF
GPIOA->AFR[0] |= (5<<20 | 5<<24 | 5<<28 | 5<<16); //setting AF05 for MOSI,MISO and SCK
SPI1->CR1 &=~(SPI_CR1_SPE);
SPI1->CR1 |= (3<<3); //Mode0
SPI1->CR1 &=~ (SPI_CR1_MSTR | SPI_CR1_SSI | SPI_CR1_SSM);
SPI1->CR1 |= SPI_CR1_SPE; //SPI enable
}
char SPI_read(void)
{
char data;
while(!(SPI1->SR & SPI_SR_RXNE));
while(SPI1->SR & SPI_SR_BSY);
data = SPI1->DR;
return data;
}
void SPI_write(char data)
{
SPI1->DR = data;
while(!(SPI1->SR & SPI_SR_TXE));
while(SPI1->SR & SPI_SR_BSY);
}
void SPI_writestring(char* str)
{
int len= strlen(str);
for(int i=0; i<len; i++)
{
SPI_write(str[i]);
}
}
void delayms(int count)
{
int i;
SysTick->LOAD = 16000; //16000 cycles in 1 ms
SysTick->VAL = 0; //reset current value to 0
SysTick->CTRL = 5; //clksource = internal. counter enabled. interrupt disabled
for(i=0; i<count; i++) //repeat 1ms cycles count number of times
{
while((SysTick->CTRL & 0x10000)==0){} //do nothing till Countflag becomes 1
}
SysTick->CTRL=0; //disable counter
}
void uart_txchar(char c)
{
while((USART2->SR & (1<<7))==0);
USART2->DR = (c);
}
char uart_rx(void)
{
char c;
while((USART2->SR & 1<<5)==0); //while RXNE ==0 (data not received) don't do anything
c = (USART2->DR);
return c;
}
void uart_txstr(char* string)
{
while(*string)
{
uart_txchar(*(string++));
}
}
void UART_init(void)
{
RCC->APB1ENR |= 1<<17; //USART2 clock enable
RCC->AHB1ENR |= 1; //Port A clock enable
GPIOA->AFR[0] |= 0x7700; //GPIOA AF7 = USART2, portA2 and PORTA3 have UART afs
GPIOA->MODER |=1<<5 | 1<<7;
USART2->BRR = 0X683;
USART2->CR1 |= 1<<3 | 1<<2; //TX Enable RX enable
USART2->CR1 |= 1<<13; //UART enable
}
void delayus(int count)
{
int i;
SysTick->LOAD = 16; //4000 cycles in 1 ms
SysTick->VAL = 0; //reset current value to 0
SysTick->CTRL = 5; //clksource = internal. counter enabled. interrupt disabled
for(i=0; i<count; i++) //repeat 1ms cycles count number of times
{
while((SysTick->CTRL & 0x10000)==0){} //do nothing till Countflag becomes 1
}
SysTick->CTRL=0; //disable counter
}
void dma_spi_read(char* buff)
{
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN | RCC_AHB1ENR_DMA2EN; //enable clock to PortA
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; //enable clock to SPI1
SPI1->CR2 |= SPI_CR2_RXDMAEN;
//DMA2 , Stream2 Channel 3
DMA2_Stream2->CR |= 3<<25 | DMA_SxCR_CIRC | DMA_SxCR_TCIE | DMA_SxCR_MINC ;
DMA2_Stream2->NDTR = 7;
DMA2_Stream2->PAR = (uint32_t)&SPI1->DR;
DMA2_Stream2->M0AR = (uint32_t)buff;
//SPI1->CR1 &= ~(1<<6);
SPI1->CR1 &=~(SPI_CR1_SPE);
SPI1->CR1 |= (3<<3); //Mode0
//SPI1->CR1 &=~(1<<11);
//SPI1->CR2 |= 0; //Motorola Frame format
SPI1->CR1 |= SPI_CR1_SPE; //SPI enable
GPIOA->MODER &= ~(3<<14 | 3<<10 | 3<<12 | 3<<8); //clear SPI bits
GPIOA->MODER |= (2<<10 | 2<<14 | 2<<12 | 2<<8 ); //set MOSI,MISO,SCK bits for AF and NSS as GPO
GPIOA->PUPDR |= 1<<14;
GPIOA->AFR[0] &= ~(0xF<<20 | 0xF<<24 | 0xF<<28); //clear AF
GPIOA->AFR[0] |= (5<<20 | 5<<24 | 5<<28 | 5<<16); //setting AF05 for MOSI,MISO and SCK
}
If I run the code on either side of "**************" line individually it works correctly, I get the correct string on PC terminal.
But with the code shown above, this is what I get
On master side:
On slave side:
The slave side seems to be receiving it somewhat correctly, while the master is receiving absolutely wrong message.
What I am doing wrong?
2020-04-07 8:00 AM
The master side
The slave side
Calling uart_txstr() in the slave loop guarantees that the slave is always late to the party, and can't respond in time.
> Assume all functions called work correctly.
Define correctly.
How long does delayms(1) wait? Hint: if it is dependent in some way on a counter variable which is incremented by a timer interrupt, then it is not exactly 1 ms, but either between 0 ms and 1 ms, or between 1 ms or 2 ms.
What does SPI_write() do? Does "work correctly" imply that it is not only putting a byte into the transmit register when it becomes empty, or there is a free slot in the transmit fifo, or does it actually wait for a byte to appear in the receive data register? What does it check after writing the data register?
What does SPI_read() do? Does "work correctly" imply that it is checking the transition of CS, and flushing the input buffer when necessary?
2020-04-07 8:32 AM
You aren't operating in true full duplex SPI mode. Data is transferred in both directions at the same time, based on clock edge. The master SPI supplies the clock and begins the transmission. At each edge a bit is clocked from the master TX register into the slave RX register, while the slave TX buffer is clocked into the master RX buffer. This works best with DMA to handle actual data transfers, assuming it's fixed length. Don't think of SPI as a fast UART; it operates in a synchronous mode where both sides set up the data exchange in advance.
This method takes less than half the time to communicate between the two boards compared to your algorithm, and far less CPU time if you use DMA.
Jack Peacock
2020-04-07 8:40 AM
Well yeah I guess to call it working fine is pretty vague. My SPI_write() and SPI_read are simple functions. They just wait for transmit buffer to get empty, wait if SPI line is BUSY and then write to or read from data register. I'll just edit the post to write the whole code.
2020-04-07 8:47 AM
I did try using DMA for reception, but it didn't help. Anyway I am trying to do everything without DMA, which I myself don't like, but the professor I am supposed to submit my report to doesn't like the idea of using DMA and wants everything be done manually checking status registers.
2020-04-07 12:20 PM
It indeed is timing issue as you said. I calculated the approximate time I am losing sending data to PC over UART and it's couple of ms at 9600 bps. So I added small delays before and after sending data from master and now I am getting better data than before. It is shifted by 4 bytes so the order is wrong, but still much better than before. And yes the clock offered by master ain't super accurate, so syncing is pretty difficult. Is DMA is the only way to go about this as another member commented on this post?