cancel
Showing results for 
Search instead for 
Did you mean: 

RM0440, Rev 7, STM32G474 Reference Manual - Errors

Singh.Harjit
Senior II

Figure 188, Page 853: The last waveform (HRTIM_REPxR = 2) should be: 1, 0, 2, 1, 0 and not 1, 0, 2, 0.

Figure 254, Page 933: For the last two waveforms (ADCxPSC[4:0]=4 ADROM[1:0]=01 and ADCxPSC[4:0]=4 ADROM[1:0]=10), it seems like the waveforms as shown are for ADCxPSC[4:0]=2.

The ADROM description at the bottom of page 932 says:

• ADROM[1:0] = 01: event generated during down-counting phases

• ADROM[1:0] = 10: event generated during up-counting phases

The pictures show ADCxPSC[4:0] counting for both edges.

I think I checked the STM32F3 that has the HRTIM and it has the same issue for the equivalent Figure 254. I didn't check the STM32H7 series reference manual or for Figure 188 equivalent in other STM32 products.

1 REPLY 1
Bubbles
ST Employee

Hello @Singh.Harjit​ ,

I'll check these problems and mark them for correction.

Thank you for your help.

BR,

Jarda

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.