2022-10-28 05:59 AM
I understand that there's a great deal of copypasting when creating RMs, but can ST please pay more attention to the details?
In particular, no part described by RM0394 should have SAI2 implemented:
yet there are references to SAI2 through the document:
All I did was textual search for SAI2 (and yes, there's also the very confusingly named but existing PLLSAI2CLK signal).
JW
2022-10-28 09:14 AM
Hello @Community member,
Thanks for reporting the issue. An internal ticket has been submitted.
Internal ticket number: 137777 (This is an internal tracking number and is not accessible or usable by customers).
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-28 12:00 PM
Thanks, @F.Belaid .
What a nice ticket number! :-)
Jan