cancel
Showing results for 
Search instead for 
Did you mean: 

RM0091 typo (OVF)

In RM0091 rev.9, footnote 2 to Figure 273 on Page 760 has the following text:

All the events associated with the transmitter receive flow must be ignored in standard transmit only mode (e.g. OVF flag).

There is no OVF flag in the 'F0xx SPI; this should probably be the OVR flag instead.

JW

1 ACCEPTED SOLUTION

Accepted Solutions
Amira
Associate III

Hello @Community member​ 

Yes you're right there is a typo here. It should be OVR flag.

This will be escalated internally in order to be fixed.

Regards,

Amira

View solution in original post

2 REPLIES 2
Amira
Associate III

Hello @Community member​ 

Yes you're right there is a typo here. It should be OVR flag.

This will be escalated internally in order to be fixed.

Regards,

Amira

Thanks, Amira.

Jan