2021-07-13 9:26 AM
In RM0091 rev.9, footnote 2 to Figure 273 on Page 760 has the following text:
All the events associated with the transmitter receive flow must be ignored in standard transmit only mode (e.g. OVF flag).
There is no OVF flag in the 'F0xx SPI; this should probably be the OVR flag instead.
JW
Solved! Go to Solution.
2021-07-13 12:19 PM
Hello @Community member
Yes you're right there is a typo here. It should be OVR flag.
This will be escalated internally in order to be fixed.
Regards,
Amira
2021-07-13 12:19 PM
Hello @Community member
Yes you're right there is a typo here. It should be OVR flag.
This will be escalated internally in order to be fixed.
Regards,
Amira
2021-07-13 12:53 PM
Thanks, Amira.
Jan