2024-12-11 04:12 AM - last edited on 2024-12-11 04:22 AM by Andrew Neil
Do I need to use RK043FN8H-CT672B for STM32F756BGT6?
Solved! Go to Solution.
2024-12-11 10:36 AM
Hello @Mimikakarlo and welcome to the community,
According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.
For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"
Hope it helps.
2024-12-11 04:23 AM
2024-12-11 09:56 AM
yes
2024-12-11 10:07 AM
I want to ask if i can use a display like this one https://gr.mouser.com/ProductDetail/Display-Visions/EA-R480X-43ALW?qs=iLbezkQI%252Bsi%2FClyHHYaCsg%3D%3D&srsltid=AfmBOoodyGLjKmbsFHHIOZ-hTdkwMIWfCXzlXGDOmeuZDaUc-w6XSSx5
because i need 1000cm/m2 brightness
2024-12-11 10:20 AM
You'd own the task of writing the driver for the SC7283, and making the determination. Looks like its probably workable.
https://www.orientdisplay.com/pdf/SC7283.pdf
2024-12-11 10:36 AM
Hello @Mimikakarlo and welcome to the community,
According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.
For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"
Hope it helps.
2024-12-11 10:46 AM
Thank you for youe answer. I have a problem with the RK043FN66HS-CTG display because i want brightness 1000cm/m^2, can you suggest me another display for STM32F756BGT6 with 4.3in, 480 x 272 pixels and 1000cm/m^2?
Thank you!
2024-12-11 02:42 PM - edited 2024-12-11 02:43 PM
This is what is used on STM32H743-Eval board: AM-640480G5TNQW-T00H