cancel
Showing results for 
Search instead for 
Did you mean: 

Problems between STM32F413 and ICM42688 using SPI

SpeedyPLH
Associate II

HI All, 

I am trying to connect an STM32F413 and the TDK ICM-42688 IMU chip using SPI.  The connection works correctly and the ICM-42688 responds, but the data doesnt seem to be clocked into the STM32F413 chip.   

The ICM-42688 Timing data is:

ICM42688 SPI Timing.png

 So CPOL = 1, CPHA = 2 and SCLK ic high in idle.

(I have also tried CPOL = 1 and CPHA = 1  which also delivers an identical result)

The Device Config is as follows:  

hspi1.Instance = SPI1;

hspi1.Init.Mode = SPI_MODE_MASTER;

hspi1.Init.Direction = SPI_DIRECTION_2LINES;

hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;

hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;

hspi1.Init.NSS = SPI_NSS_SOFT;

hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;

hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi1.Init.CRCPolynomial = 10;

 

SpeedyPLH_0-1713325909638.png

I have it slowed down at present to see if speed is the cause of my problems...

 

When I monitor the lines with my Saleae 16 I get a good response.

ICM42688 SPI Timing Saleae.png

The 0x76,00 is a write to the register 0x76 to select bank 0.

The 0xF5,00 is a read request for the Register 0x75 and it should return 0x47 which is is doing - YAY.

My problem is that the data doesnt seem to be clocked into the STM32F413 chip...

I always end up with 0x00.

I have tried a number of different permutations using HAL_SPI_Read and HAL_SPI_TransmitReceive and none seem to work.

Here is the code doing the work.

 

 
const uint16_t SPI_TIMEOUT = 100; // 100 ms
static constexpr uint8_t WHOAMI = 0x47;
 
uint8_t CSpiDevice::_readRegister(uint8_t *recv, uint16_t rLen)
{
uint8_t result = HAL_OK;
HAL_GPIO_WritePin(_pGPIO, _CS, GPIO_PIN_RESET);
// result = HAL_SPI_Receive((SPI_HandleTypeDef*)get_handle(), recv, (uint16_t)rLen, SPI_TIMEOUT);
result = HAL_SPI_TransmitReceive ((SPI_HandleTypeDef*)get_handle(), recv, recv, rLen, SPI_TIMEOUT);
HAL_GPIO_WritePin(_pGPIO, _CS, GPIO_PIN_SET);
return result == HAL_OK ? OK : ERR;
}
 
template <typename T>
uint8_t Cicm42688P::RegisterRead(T reg)
{
uint8_t cmd[2] {};
cmd[0] = static_cast<uint8_t>(reg) | DIR_READ;
SelectRegisterBank(reg);
if(_readRegister(cmd, sizeof(cmd))!= OK)
INFO_LOG(logger::CdataLog::errorCategory_e::data_error,sRReadErr,RReadErrLn,0);
return cmd[1];
}
 
static const char sProbeError[] = "probe() Returned (0x%hx)";
static constexpr uint8_t probeErrorLn = strlen(sProbeError);
 
uint8_t Cicm42688P::probe(void) {
SelectRegisterBank(REG_BANK_SEL_BIT::BANK_SEL_0, true);
uint8_t whoami = RegisterRead(Register::BANK_0::WHO_AM_I);
if (whoami == WHOAMI) {
INFO_LOG(logger::CdataLog::errorCategory_e::information_only,
sProbeError, probeErrorLn,whoami);
return OK;
 
} else {
INFO_LOG(logger::CdataLog::errorCategory_e::configuration_error,
sProbeError, probeErrorLn,whoami);
}
return ERR;
};

 

I am somewhat flumoxed at present.

Any and all thoughts are appeciated.  

Thanks in Advance.

 

cheers

Paul

4 REPLIES 4
SpeedyPLH
Associate II

Sorry Typo . 0x75 is a register in Bank 0. 

Amit29
Associate

Hey can u share the code for the driver , I am currently working on a project and i need the drivers code very urgently 

kindly share the libarary you used to interface the ICM-42688P 

Techn
Senior II

Spi_TransmitReceive , you have to fill with the register value and then dummy bytes of zero to clock out the data. For example 

rx[0] = 0x75; rx[1] = 0  till the len count. 

FYI. As per datasheet, the first bit should be 1 for read and 0 for write. So you can try eith 0xF5

sir do you have the code for ICM42688 for interfacing with stm32 ?? if yes ,kindly share it.