cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with STM32L475 Discovery kit IoT node power supply

DMala.1
Associate II

Hello, I've just received the STM32L475 Discovery kit IoT node. I connected the board through USB cable to my laptop (the JP4 jumper is connected to 5V_ST_LINK) and the power supply LED (LD5) is blinking. Also the board is not visible from laptop (I have installed the required drivers). What is going on? Is there something else I have to do?

4 REPLIES 4

Make sure not to use a charging cable, these only have power lines, and lack the data lines for connectivity.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Evangelist III

> Also the board is not visible from laptop (I have installed the required drivers).

Are you sure? Have you looked in Devices and Printers, or used a tool such as USBview?

-- pa

Hi, thank you for your answer. The problem seems to be the power supply, that's why the board is not visible. The power supply LED should be on and not blinking. ​

Hi, thank you for your answer. The problem seems to be the power supply, that's why the board is not visible. The power supply LED should be on and not blinking. ​