2017-07-28 11:16 AM
Hello
I'm using a Nucleo-F413ZH board with System Workbench for STM32, Currently I try to startup the FSMC Interfcae 16 Bit for my QVGA Display with SSD2119. I config the Ports and the FSMC peripheral OK DB15 (PD10 is not Connected on Nucelon Board here I made a wire connection to the µC) . FSMC is located to Bank1 D0 - D15 are ok, but on D14 connected on PD9 I measure a permanent high, can anyone imagine why? I check my soldering contact on PD10 with a microscope and everything looks good.
Thanks for your help
Daniel
Solved! Go to Solution.
2017-07-28 11:37 AM
Hello!
PD9 is connected to stlink TX (serial port.)
Remove the jumper SB6
2017-07-28 11:37 AM
Hello!
PD9 is connected to stlink TX (serial port.)
Remove the jumper SB6
2017-07-29 01:14 AM
Thanks, That PD9 is connected via SB6 I had overlooked completely
But I understand the schematic and the datasheet correct, I can remove SB6 and I didn't need STLK_TX for communication with the Nucleon-Board, because
I use the USB Connection. Please improve me if I'm wrong
Best regards
Daniel