cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with PD9 by FSMC Interface on Nucleo-F413ZH board

Daniel Homes
Associate
Posted on July 28, 2017 at 20:16

Hello

I'm using a Nucleo-F413ZH board with System Workbench for STM32, Currently I try to startup the FSMC Interfcae 16 Bit for my QVGA Display with SSD2119. I config the Ports and the FSMC peripheral OK DB15 (PD10 is not Connected on Nucelon Board here I made a wire connection to the µC) . FSMC is located to Bank1 D0 - D15 are ok, but on D14 connected on PD9 I measure a permanent high, can anyone imagine why? I check my soldering contact on PD10 with a microscope and everything looks good. 

Thanks for your help

Daniel

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on July 28, 2017 at 20:37

Hello!

PD9 is connected to stlink TX (serial port.)

Remove the jumper SB6

View solution in original post

2 REPLIES 2
Posted on July 28, 2017 at 20:37

Hello!

PD9 is connected to stlink TX (serial port.)

Remove the jumper SB6

Daniel Homes
Associate
Posted on July 29, 2017 at 10:14

Thanks,  That PD9 is connected via SB6 I had overlooked completely

But I understand the schematic and the datasheet correct, I can remove SB6 and I didn't need STLK_TX for communication with the Nucleon-Board, because

I use the USB Connection. Please improve me if I'm wrong

Best regards

Daniel