cancel
Showing results for 
Search instead for 
Did you mean: 

SDIO INTERFACES IN STM32F407VG

vinayashree k s
Associate II
Posted on July 25, 2017 at 13:16

HOW MANY SDIO INTERFACES ARE THEIR IN STM32F407VG ????ONLY ONE OR TWO??IF TWO ARE THEIR CAN I USE BOTH AT SAME TIME??       

https://community.st.com/community/stm32-community/stm32-forum?sr=search&searchId=521dc8c2-71bb-41b0-99e0-215e18448dff&searchIndex=0

#stm32f407vg
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on July 26, 2017 at 10:52

Hello !!

According to dataseet There is only one exist.

View solution in original post

7 REPLIES 7
Posted on July 26, 2017 at 10:52

Hello !!

According to dataseet There is only one exist.

vinayashree k s
Associate II
Posted on July 26, 2017 at 11:49

THANK YOU

I WANT TO KNOW IS THEIR ANY STM32F4 SERIES BOARD WHICH IS HAVING 2 SDIO INTERFACES????

IN STM32F7 SERIES 2 SDIO INTERFACES ARE AVAILABLE,CAN I USE BOTH INTERFACES AT SAME TIME???

FORTOUNAS.EVANGELOS

Amel NASRI
ST Employee
Posted on July 26, 2017 at 12:13

Please keep discussing in same thread:

https://community.st.com/0D50X00009XkXUnSAN

.

No need for topic duplication.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on July 26, 2017 at 12:11

Take a look at

https://my.st.com/content/my_st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32-high-performance-mcus/stm32f4-series.html?querycriteria=productId=SS1577

.  for the  first question.

For the second , Any peripheral can be used same time with any other peripheral;

Exceptions

pin availability for exclusive or shared use from each peripheral

Errata sheet limitations.

By definition from ST writen clear in ref manual (no company wants this kind of limitation for their products)

Posted on July 26, 2017 at 13:16

Can we also try not to type in ALL CAPS, the Internet considers this to be shouting 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
vinayashree k s
Associate II
Posted on July 27, 2017 at 05:58

i got this information in datasheet of one of STM32F7 board

The current version supports only one SD/SDMMC/MMC4.2 card at any one time and a stack of MMC4.1 or previous.

what does it means????As we have separate pins for both interfaces ,i can communicate using 2 sdio pins with different devices at same time?????

st.mcu

FORTOUNAS.EVANGELOS

Posted on July 28, 2017 at 23:54

Hi!!

STM32F779BIT (at least) can communicate using 2 sdmmc at same time.

STM32F769NIH,,