cancel
Showing results for 
Search instead for 
Did you mean: 

Possible error in RM0444 REV_ID for STM32G071xx and STM32G081xx

MikeG
Associate

Hello everyone,

I wanted to ask if this is an error or if this is documented right:

When you take a look in the latest RM0444 Rev 5 reference manual on page 1373 there are the DBG registers explained. The "DBG device ID code register (DBG_IDCODE)"  for the STM32G071xx and STM32G081xx do have for the Revision Code Z and Revision Number 1.1 the REV_ID 0x1000. The same REV_ID is used for Revision code A and Revision number 1.0. I attached a screenshot of the manual.

Is this a typo or do they really have the same REV_ID for Revision code A and Z?

On the next page, the devices G031 and G041 are described, here with differing REV_ID`s. I think this should be the same for STM32G071xx.

Please let me know, if my assumption is true. And if this is not a typo, is there a way to find out what Revision number/code my G071 MCU does actually have?

Thanks in advance,

Michael

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @MikeG ,

Getting back to you as I had a feedback regarding your case and confirms that this is not a typo and RevA / RevZ have indeed the same REV ID value. In fact it was an exception for a internal manufacturing reasons.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
SofLit
ST Employee

Hello @MikeG ,

It will be escalated for verification. Internal ticket 197665 for tracking. I'll get back to you as soon as I have an answer.

Thanks.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
SofLit
ST Employee

Hello @MikeG ,

Getting back to you as I had a feedback regarding your case and confirms that this is not a typo and RevA / RevZ have indeed the same REV ID value. In fact it was an exception for a internal manufacturing reasons.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.