2025-08-04 9:02 AM - edited 2025-08-04 9:07 AM
When flashing the STM32L431CCT6 (Device ID=0x435) using STM32CubeIDE v1.19, the MCU intermittently fails to boot from user flash (0x08000000), instead jumping to system memory (around 0xfff1...). This causes the Reset_Handler to crash or fail. Downgrading to STM32CubeIDE v1.18.1 resolves the issue, suggesting a flash loader bug in v1.19.
Non working:
CubeIDE version: 1.19.0
Cubeprogrammer version: 2.20.0
Working:
CubeIDE version: 1.18.1
Cubeprogrammer version: 2.19.0
Symptoms:
Flashing with STM32CubeIDE v1.19 results in intermittent failures, with the MCU breaking at addresses around 0xfff1... (system memory).
The Reset_Handler sometimes crashes, likely due to incorrect booting.
The issue is consistent on one laptop (v1.19) but absent on another (v1.18.1).
Cause: Per a previous ST Community post, the PEMPTY flag is maybe not being cleared properly by the flash loader, causing the STM32L431CCT6 to boot into system memory instead of user flash. Reference: [ST Community thread mentioning flash loader patches for STM32L4 series].