cancel
Showing results for 
Search instead for 
Did you mean: 

On STM32H7, can DMA access generate an ECC error ?

PBard.2
Associate

Hello,

I am currently working with stm32H743 processor.

I wanted to know if DMA access can trigger an ECC error or only the core can generate these errors.

For example if there is a ram data protected by ECC with a double bit error, would a DMA access to this corrupted data generate a bus fault error ?

Thanks

Regards

1 REPLY 1

> I wanted to know if DMA access can trigger an ECC error

I see no reason why not.

JW