cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-H743ZI2 FDCAN: late trigger of Rx interrupts

KT_Matt
Associate II

(Moved to appropriate forum from 'Feedback')

 

Hi,

I'm using Nuleo-H743Zi2 hardware. I have configured FDCAN1 with below configurations,

hfdcan1.Instance = FDCAN1; hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS; hfdcan1.Init.Mode = FDCAN_MODE_NORMAL; hfdcan1.Init.AutoRetransmission = ENABLE; hfdcan1.Init.TransmitPause = DISABLE; hfdcan1.Init.ProtocolException = ENABLE; hfdcan1.Init.NominalPrescaler = prescaler; hfdcan1.Init.NominalSyncJumpWidth = 1; hfdcan1.Init.NominalTimeSeg1 = 13; hfdcan1.Init.NominalTimeSeg2 = 2; hfdcan1.Init.DataPrescaler = 1; hfdcan1.Init.DataSyncJumpWidth = 1; hfdcan1.Init.DataTimeSeg1 = 1; hfdcan1.Init.DataTimeSeg2 = 1; hfdcan1.Init.MessageRAMOffset = 0; hfdcan1.Init.StdFiltersNbr = 0; hfdcan1.Init.ExtFiltersNbr = 0; hfdcan1.Init.RxFifo0ElmtsNbr = 8; hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxFifo1ElmtsNbr = 8; hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxBuffersNbr = 8; hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.TxEventsNbr = 8; hfdcan1.Init.TxBuffersNbr = 8; hfdcan1.Init.TxFifoQueueElmtsNbr = 8; hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION; hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8; if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN FDCAN1_Init 2 */ FDCAN_FilterTypeDef sFilterConfig; sFilterConfig.IdType = FDCAN_STANDARD_ID; sFilterConfig.FilterIndex = 0; sFilterConfig.FilterType = FDCAN_FILTER_MASK; sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0; sFilterConfig.FilterID1 = 0x400; sFilterConfig.FilterID2 = 0x5FF; if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK) { // Filter configuration Error Error_Handler(); } if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK) { // Start Error Error_Handler(); } if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_COMPLETE | FDCAN_IT_RX_FIFO0_NEW_MESSAGE | FDCAN_IT_BUS_OFF | FDCAN_IT_ERROR_PASSIVE | FDCAN_IT_ERROR_WARNING, 0) != HAL_OK) { // Notification Error Error_Handler(); } ***************************************************************************************************** ***************************************************************************************************** GPIO_InitTypeDef GPIO_InitStruct = {0}; RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0}; if(hfdcan->Instance==FDCAN1) { /* USER CODE BEGIN FDCAN1_MspInit 0 */ /* USER CODE END FDCAN1_MspInit 0 */ /** Initializes the peripherals clock */ PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_FDCAN; PeriphClkInitStruct.PLL2.PLL2M = 8; PeriphClkInitStruct.PLL2.PLL2N = 48; PeriphClkInitStruct.PLL2.PLL2P = 2; PeriphClkInitStruct.PLL2.PLL2Q = 8; PeriphClkInitStruct.PLL2.PLL2R = 2; PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3; PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE; PeriphClkInitStruct.PLL2.PLL2FRACN = 0; PeriphClkInitStruct.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL2; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { Error_Handler(); } /* Peripheral clock enable */ __HAL_RCC_FDCAN_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); /**FDCAN1 GPIO Configuration PD0 ------> FDCAN1_RX PD1 ------> FDCAN1_TX */ GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); /* FDCAN1 interrupt Init */ HAL_NVIC_SetPriority(FDCAN1_IT0_IRQn, 1, 0); HAL_NVIC_EnableIRQ(FDCAN1_IT0_IRQn); /* USER CODE BEGIN FDCAN1_MspInit 1 */ /* USER CODE END FDCAN1_MspInit 1 */ }
View more

The FDCAN Reception interrupts are triggered late >500ms sometimes more than a second. So the requests from master gets timed out.

a. Is the above configuration is correct?

b. If yes, what can be done to improve the performance?

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @KT_Matt ,

I would suggest these timings @500kb/s for FDCAN in classic mode/ MCU running at 400MHz with an extarnal precise crystal (in your case 8MHz using STLINK MCO in Bypass mode):

SofLit_0-1731918663795.png

SofLit_1-1731918722625.png

SofLit_2-1731918757056.png

I've attached the updated ioc file.

Hope it helps.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

15 REPLIES 15
mÆŽALLEm
ST Employee

Hello @KT_Matt

To share your code please use </> button. Tips on posting.

At a first glance and according to you config, you are using FDCAN mode and these data phase parameter timings are bad: BS1 = 1, BS2 = 1.

 

hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS; hfdcan1.Init.Mode = FDCAN_MODE_NORMAL; hfdcan1.Init.DataPrescaler = 1; hfdcan1.Init.DataTimeSeg1 = 1; hfdcan1.Init.DataTimeSeg2 = 1;

 

Need to increase BS1 and BS2 as much as possible and decrease the prescaler to match your data phase bitrate.

Please refer to this article. It gives an example of FDCAN communication on Nucleo-H7 with Nominal phase bitrate = 1Mb/s and the data phase at 8Mb/s. And provided an example of calculation.

Are you sure the other node is in FDCAN mode not in classic mode?

What is the bitrate you are using for both nominal and data phase?

Could you please share your ioc file?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi @mÆŽALLEm,

Thanks for responding.

My requirement is for Classic Mode only  and the bitrate needed is 125, 250, 500Kbps. For classic mode, the recommended changes are needed?

Attached the ioc file. 

Thanks and Regards

 

I would suggest to use a CAN trace tool (or a scope), to check what is really happening on the bus, and when.

Hi @Ozone ,

We used CAN trace, the CAN messages are received at the Hardware queue, but the interrupt is not triggered or triggered late(>500ms). If the interrupt not triggered means, later when interrupt triggers, the previous message gets handled. 

Hello @KT_Matt ,

I would suggest these timings @500kb/s for FDCAN in classic mode/ MCU running at 400MHz with an extarnal precise crystal (in your case 8MHz using STLINK MCO in Bypass mode):

SofLit_0-1731918663795.png

SofLit_1-1731918722625.png

SofLit_2-1731918757056.png

I've attached the updated ioc file.

Hope it helps.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Ok, I understand.
Occasionally, some poster here need to be reminded that CAN is not a deterministic bus, and a CAN trace or such is necessary.

> ... the CAN messages are received at the Hardware queue, but the interrupt is not triggered or triggered late(>500ms).

This suggests it is an issue with the H743's CAN peripheral, which I have no actual experience with.

Hi @mÆŽALLEm ,

I tried the recommended configuration. Looks like the FDCAN is not working with this clock speed(100Mhz). It works only with 48MHz. 

Hello @KT_Matt ,

It should work at 100MHz / System clock at 400MHz/VOS1:

SofLit_0-1731923794855.png

Did you try Loopback mode first? Try External Loopback mode and probe with an oscilloscope or analyzer on FDCAN_Tx pin. Do you receive the sent frame?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Also could you please check if the HSE is 8MHz?

For that you need to check that on MCO1 (PA8). I've attached the ioc file where I've added the output of HSE on PA8.

Could you please check with an oscilloscope if you have 8MHz on PA8?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.