cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-G474RE -multimode -dual regular simultaneous - ADC2 is not working properly

mgdudhat
Associate

Hi all,

I am working on Nucleo-G474RE board to get the ADC result in multimode-continuous conversion- -dual regular simultaneous (ADC1-two channels  (1,2) & ADC2-two channels (3,4)) with DMA transfer (peripheral to memory). Here I checked the buffer value with word (data width) setting done in DMA configuration. The code was generated from STM32cubeMx after required setting.

Unfortunately only ADC1 value is getting changed every time and rest half word -ADC2 value is showing always fixed everytime. Could you please let me know why this thing is happening. You advices are welcome. Thank you.

 

 

1 REPLY 1
SofLit
ST Employee

Hello @mgdudhat and welcome to the community.

Need to share more details especially your code to let community members to help you efficiently.

Also, please review the tips on how to post a thread in this link.

Thank you. 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.